![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
Linear Technology DC939A Demonstration Board. More...
Linear Technology DC939A Demonstration Board.
LTC2484: 24-Bit Delta Sigma ADC with Easy Drive Input Current Cancellation.
NOTES
Setup:
Set the terminal baud rate to 115200 and select the newline terminator. Equipment
required is a precision voltage source and a precision voltmeter. No external
power supply is required. Ensure JP1 is in the +5V position.
To Read data:
The voltage source should be connected with positive lead to IN+ and negative
lead to IN-. The voltage source negative output must also be connected to the GND
pin in order to provide a ground-referenced voltage. Ensure voltage is within
analog input voltage range -0.3V to +2.5V. Swapping input voltages results in a
reversed polarity reading.
How to calibrate:
Short the inputs to ground to calibrate the offset. Next, hit ENTER (this takes
the reading). Now apply approximately 2.49 volts to +IN, with -IN connected to
ground. Measure this voltage with a precise voltmeter and enter this value.
Calibration is now stored in EEPROM. Upon startup the calibration values will be
restored.
Explanation of Commands:
**** MAIN MENU ****
0- Read- By entering this a voltage at the +IN, -IN terminals will be read.
1- Set Rejection- Select this to access the Filter rejection menu. Follow
command cues to enable desired rejection profile of on-chip digital filters.
2- Select 2X Rate- This selection allows disabling of the autocalibration
feature to achieve a benefit of twice the output rate.
3- Calibrate Voltage- Follow the calibration cues to calibrate the device
voltage.
4- Calibrate Temperature- Select this and follow the cues if it is desired to
calibrate the integrated
temperature sensor.
USER INPUT DATA FORMAT:
decimal : 1024
hex : 0x400
octal : 02000 (leading 0 "zero")
binary : B10000000000
float : 1024.0http://www.linear.com/product/LTC2484
http://www.linear.com/product/LTC2484#demoboards
Copyright 2018(c) Analog Devices, Inc.
All rights reserved.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
THIS SOFTWARE IS PROVIDED BY ANALOG DEVICES "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, NON-INFRINGEMENT, MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL ANALOG DEVICES BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, INTELLECTUAL PROPERTY RIGHTS, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
Definition in file DC939A.ino.
Go to the source code of this file.
Functions | |
| static void | print_title () |
| Prints the title block when program first starts. More... | |
| static void | print_prompt () |
| Prints main menu. More... | |
| static int8_t | restore_calibration () |
| Read stored calibration parameters from nonvolatile EEPROM on demo board. More... | |
| static void | store_calibration () |
| Store measured calibration parameters to nonvolatile EEPROM on demo board. More... | |
| static uint8_t | build_adc_command (uint8_t temperature) |
| Construct ADC command from rejection, input, and 2X parameters. More... | |
| static uint8_t | menu_0_read () |
| Read ADC. More... | |
| static void | menu_1_set_rejection () |
| Set rejection mode. More... | |
| static void | menu_2_set_1X_2X () |
| Select 1X or 2X mode. More... | |
| static uint8_t | menu_3_calibrate_voltage () |
| Calibrate ADC given two known inputs. More... | |
| static uint8_t | menu_4_calibrate_temperature () |
| Calibrate Temperature given two known inputs. More... | |
| static void | setup () |
| Initialize Linduino. More... | |
| static void | loop () |
| Repeats Linduino loop. More... | |
Macros | |
| #define | REJECTION50_60 0 |
| 50-60Hz rejection More... | |
| #define | REJECTION50 1 |
| 50Hz rejection More... | |
| #define | REJECTION60 2 |
| 60Hz rejection More... | |
Variables | |
| static uint8_t | demo_board_connected |
| Set to 1 if the board is connected. More... | |
| static int8_t | adc_rejection = REJECTION50_60 |
| The LTC2484 rejection. More... | |
| static int8_t | adc_2x = 0 |
| The LTC2484 2x speed mode. More... | |
| static float | LTC2484_lsb = 9.3132258E-9 |
| Ideal LSB size, 5V/(2^29) for a 5V reference. More... | |
| static int32_t | LTC2484_offset_code = 0 |
| Ideal offset. More... | |
| static float | LTC2484_t0 = 27.0 |
| Nominal temperature. More... | |
| static float | LTC2484_r0 = 45.097156E6 |
| ADC code at the nominal temperature (420mV default) More... | |
| const uint16_t | MISO_TIMEOUT = 1000 |
| The MISO timeout (ms) More... | |
|
static |
Construct ADC command from rejection, input, and 2X parameters.
Definition at line 297 of file DC939A.ino.
|
static |
Repeats Linduino loop.
Definition at line 158 of file DC939A.ino.
|
static |
|
static |
Set rejection mode.
Definition at line 374 of file DC939A.ino.
|
static |
Select 1X or 2X mode.
Definition at line 402 of file DC939A.ino.
|
static |
Calibrate ADC given two known inputs.
Definition at line 427 of file DC939A.ino.
|
static |
Calibrate Temperature given two known inputs.
Definition at line 477 of file DC939A.ino.
|
static |
Prints main menu.
Definition at line 219 of file DC939A.ino.
|
static |
Prints the title block when program first starts.
Definition at line 203 of file DC939A.ino.
|
static |
Read stored calibration parameters from nonvolatile EEPROM on demo board.
Definition at line 260 of file DC939A.ino.
|
static |
Initialize Linduino.
Definition at line 139 of file DC939A.ino.
|
static |
Store measured calibration parameters to nonvolatile EEPROM on demo board.
Definition at line 284 of file DC939A.ino.
| #define REJECTION50 1 |
50Hz rejection
Definition at line 109 of file DC939A.ino.
| #define REJECTION50_60 0 |
50-60Hz rejection
Definition at line 108 of file DC939A.ino.
| #define REJECTION60 2 |
60Hz rejection
Definition at line 110 of file DC939A.ino.
|
static |
The LTC2484 2x speed mode.
Definition at line 128 of file DC939A.ino.
|
static |
The LTC2484 rejection.
Definition at line 127 of file DC939A.ino.
|
static |
Set to 1 if the board is connected.
Definition at line 126 of file DC939A.ino.
|
static |
Ideal LSB size, 5V/(2^29) for a 5V reference.
Definition at line 131 of file DC939A.ino.
|
static |
Ideal offset.
Definition at line 132 of file DC939A.ino.
|
static |
ADC code at the nominal temperature (420mV default)
Definition at line 134 of file DC939A.ino.
|
static |
Nominal temperature.
Definition at line 133 of file DC939A.ino.
| const uint16_t MISO_TIMEOUT = 1000 |
The MISO timeout (ms)
Definition at line 136 of file DC939A.ino.