![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
Linear Technology DC742A Demonstration Board. More...
Linear Technology DC742A Demonstration Board.
LTC2449: 24-Bit, 16-Channel Delta Sigma ADC with Selectable Speed/Resolution.
Linear Technology DC979A Demonstration Board. LTC2442: 24-Bit, 4-Channel Delta Sigma ADC with Integrated Amplifier
Linear Technology DC845A Demonstration Board. LTC2448: 24-Bit, 8-/16-Channel Delta Sigma ADCs with Selectable Speed/Resolution
NOTES Setup: Set the terminal baud rate to 115200 and select the newline terminator. Equipment required is a precision voltage source and a precision voltmeter. Additionally, an external power supply is required to provide a negative voltage for Amp V-. Set it to anywhere from -1V to -5V. Set Amp V+ to Vcc. Ensure the COM and REF- pins are connected to ground. The REF+ pin should be connected to +5V. How to test Single-Ended mode: The voltage source should be connected to the ADC such that the negative lead is connected to the COM(common) pin. The positive lead may be connected to any channel input. Ensure voltage is within analog input voltage range -0.3 to 2.5V. How to test Differential Mode: The voltage source should be connected with positive and negative leads to paired channels. The voltage source negative output must also be connected to the COM pin in order to provide a ground-referenced voltage. Ensure voltage is within analog input voltage range -0.3V to +2.5V. Swapping input voltages results in a reversed polarity reading. How to calibrate: Apply 100mV CH0 with respect to COM. Next, measure this voltage with a precise voltmeter and enter this value. (This takes the reading.) Now apply approximately 2.40 volts to CH0. Measure this voltage with a precise voltmeter and enter this value. Calibration is now stored in EEPROM. Upon start-up the calibration values will be restored. USER INPUT DATA FORMAT: decimal : 1024 hex : 0x400 octal : 02000 (leading 0 "zero") binary : B10000000000 float : 1024.0
http://www.linear.com/product/LTC2449 http://www.linear.com/product/LTC2442 http://www.linear.com/product/LTC2448
http://www.linear.com/product/LTC2449#demoboards http://www.linear.com/product/LTC2442#demoboards http://www.linear.com/product/LTC2448#demoboards
Copyright 2018(c) Analog Devices, Inc.
All rights reserved.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
THIS SOFTWARE IS PROVIDED BY ANALOG DEVICES "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, NON-INFRINGEMENT, MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL ANALOG DEVICES BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, INTELLECTUAL PROPERTY RIGHTS, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
Definition in file DC742A.ino.
Go to the source code of this file.
Functions | |
| static void | print_title () |
| Prints the title block when program first starts. More... | |
| static void | print_prompt () |
| Prints main menu. More... | |
| static void | print_user_command (uint8_t menu) |
| Display selected differential channels. More... | |
| static void | store_calibration () |
| Store measured calibration parameters to nonvolatile EEPROM on demo board. More... | |
| static int8_t | restore_calibration () |
| Read stored calibration parameters from nonvolatile EEPROM on demo board. More... | |
| static int8_t | menu_1_read_single_ended () |
| Read channels in single-ended mode. More... | |
| static int8_t | menu_2_read_differential () |
| Read channels in differential mode. More... | |
| static int8_t | menu_3_calibrate () |
| Calibrate ADC given two known inputs. More... | |
| static void | menu_4_set_OSR () |
| Set Oversample Ratio (OSR) More... | |
| static void | menu_5_set_1X2X () |
| Set 1X or 2X mode. More... | |
| static void | menu_6_en_dis_cal () |
| Enable / Disable calibration without actually touching stored calibration values. More... | |
| static void | setup () |
| Initialize Linduino. More... | |
| static void | loop () |
| Repeats Linduino loop. More... | |
Variables | |
| static uint8_t | demo_board_connected |
| Set to 1 if the board is connected. More... | |
| static int16_t | OSR_mode = LTC2449_OSR_32768 |
| The LTC2449 OSR setting. More... | |
| static int16_t | two_x_mode = LTC2449_SPEED_1X |
| The LTC2449 2X Mode settings. More... | |
| static float | LTC2449_lsb = 9.3132258E-9 |
| Ideal LSB voltage for a perfect part. More... | |
| static int32_t | LTC2449_offset_code = 0 |
| Ideal offset for a perfect part. More... | |
| const uint16_t | BUILD_COMMAND_SINGLE_ENDED [16] |
| Lookup table to build the command for single-ended mode. More... | |
| const uint16_t | BUILD_COMMAND_DIFF [16] |
| Lookup table to build the command for differential mode. More... | |
| const uint16_t | BUILD_OSR_COMMAND [10] |
| Lookup table to build the command for OSR. More... | |
| const uint16_t | BUILD_1X_2X_COMMAND [2] = {LTC2449_SPEED_1X, LTC2449_SPEED_2X} |
| Lookup table to build 1X / 2X bits. More... | |
| const uint16_t | MISO_TIMEOUT = 1000 |
| MISO timeout constant. More... | |
|
static |
Repeats Linduino loop.
Definition at line 175 of file DC742A.ino.
|
static |
Read channels in single-ended mode.
Definition at line 307 of file DC742A.ino.
|
static |
Read channels in differential mode.
Definition at line 396 of file DC742A.ino.
|
static |
Calibrate ADC given two known inputs.
Definition at line 494 of file DC742A.ino.
|
static |
|
static |
|
static |
Enable / Disable calibration without actually touching stored calibration values.
Definition at line 616 of file DC742A.ino.
|
static |
Prints main menu.
Definition at line 236 of file DC742A.ino.
|
static |
Prints the title block when program first starts.
Definition at line 221 of file DC742A.ino.
|
static |
Display selected differential channels.
Displaying single-ended channels is straightforward; not so with differential because the inputs can take either polarity.
Definition at line 249 of file DC742A.ino.
|
static |
Read stored calibration parameters from nonvolatile EEPROM on demo board.
Definition at line 641 of file DC742A.ino.
|
static |
Initialize Linduino.
Definition at line 157 of file DC742A.ino.
|
static |
Store measured calibration parameters to nonvolatile EEPROM on demo board.
Definition at line 605 of file DC742A.ino.
| const uint16_t BUILD_1X_2X_COMMAND[2] = {LTC2449_SPEED_1X, LTC2449_SPEED_2X} |
Lookup table to build 1X / 2X bits.
Build the command for 1x or 2x mode
Definition at line 151 of file DC742A.ino.
| const uint16_t BUILD_COMMAND_DIFF[16] |
Lookup table to build the command for differential mode.
Build the command for differential mode
Definition at line 139 of file DC742A.ino.
| const uint16_t BUILD_COMMAND_SINGLE_ENDED[16] |
Lookup table to build the command for single-ended mode.
Builds the command for single-ended mode
Definition at line 132 of file DC742A.ino.
| const uint16_t BUILD_OSR_COMMAND[10] |
Lookup table to build the command for OSR.
Build the command for OSR
Definition at line 146 of file DC742A.ino.
|
static |
Set to 1 if the board is connected.
Definition at line 123 of file DC742A.ino.
|
static |
Ideal LSB voltage for a perfect part.
Definition at line 126 of file DC742A.ino.
|
static |
Ideal offset for a perfect part.
Definition at line 127 of file DC742A.ino.
| const uint16_t MISO_TIMEOUT = 1000 |
MISO timeout constant.
Definition at line 154 of file DC742A.ino.
|
static |
The LTC2449 OSR setting.
Definition at line 124 of file DC742A.ino.
|
static |
The LTC2449 2X Mode settings.
Definition at line 125 of file DC742A.ino.