![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
Linear Technology DC726B-B (or DC726A-B) Demonstration Board. More...
Linear Technology DC726B-B (or DC726A-B) Demonstration Board.
LTC6904: 1kHz to 68MHz Serial Port Programmable Oscillator
NOTES Setup: Set the terminal baud rate to 115200 and select the newline terminator. Equipment required is a precision voltage source and a precision voltmeter (to monitor voltage source). No external power supply is required. Ensure JP1 is installed in the default position from the factory. Demo Board Configuration: To properly use this program with the DC726B-B demo board (or the DC726A-B), JMP 2 needs to be set to QuikEval. USER INPUT DATA FORMAT: decimal : 1024 hex : 0x400 octal : 02000 (leading 0 "zero") binary : B10000000000 float : 1024.0
http://www.linear.com/product/LTC6904
http://www.linear.com/product/LTC6904#demoboards
Copyright 2018(c) Analog Devices, Inc.
All rights reserved.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
THIS SOFTWARE IS PROVIDED BY ANALOG DEVICES "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, NON-INFRINGEMENT, MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL ANALOG DEVICES BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, INTELLECTUAL PROPERTY RIGHTS, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
Definition in file DC726B_B.ino.
Go to the source code of this file.
Functions | |
| static void | print_title () |
| Prints the title block when program first starts. More... | |
| static void | print_prompt () |
| Prints main menu. More... | |
| static void | settings () |
| Configures the output. More... | |
| static uint8_t | set_frequency () |
| Sets the output frequency. More... | |
| static uint8_t | manually_set_reg () |
| Manually Sets OCT and DAC Code. More... | |
| static void | setup () |
| Initialize Linduino. More... | |
| static void | loop () |
| Repeats Linduino loop. More... | |
Variables | |
| static uint8_t | output_config = LTC6904_CLK_ON_CLK_INV_ON |
| Keeps track of output configuration. More... | |
|
static |
Repeats Linduino loop.
Definition at line 101 of file DC726B_B.ino.
|
static |
|
static |
Prints main menu.
Definition at line 157 of file DC726B_B.ino.
|
static |
Prints the title block when program first starts.
Definition at line 142 of file DC726B_B.ino.
|
static |
Sets the output frequency.
Definition at line 169 of file DC726B_B.ino.
|
static |
Configures the output.
Definition at line 217 of file DC726B_B.ino.
|
static |
Initialize Linduino.
Definition at line 91 of file DC726B_B.ino.
|
static |
Keeps track of output configuration.
Definition at line 88 of file DC726B_B.ino.