![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
Linear Technology DC570A Demonstration Board. More...
Linear Technology DC570A Demonstration Board.
LTC2440: 24-Bit, Differential Delta Sigma ADCs with Selectable Speed/Resolution
NOTES Setup: Set the terminal baud rate to 115200 and select the newline terminator. Equipment required is a precision voltage source and a precision voltmeter. Additionally, an external power supply is required to provide a negative voltage for Amp V-. Set it to anywhere from -1V to -5V. Set Amp V+ to Vcc. Ensure the COM and REF- pins are connected to ground. The REF+ pin should be connected to +5V. How to test Differential Mode: The voltage source should be connected with positive and negative leads to paired channels. The voltage source negative output must also be connected to the COM pin in order to provide a ground-referenced voltage. Ensure voltage is within analog input voltage range -0.3V to +2.5V. Swapping input voltages results in a reversed polarity reading. USER INPUT DATA FORMAT: decimal : 1024 hex : 0x400 octal : 02000 (leading 0 "zero") binary : B10000000000 float : 1024.0
http://www.linear.com/product/LTC2440
http://www.linear.com/product/LTC2440#demoboards
Copyright 2018(c) Analog Devices, Inc.
All rights reserved.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
THIS SOFTWARE IS PROVIDED BY ANALOG DEVICES "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, NON-INFRINGEMENT, MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL ANALOG DEVICES BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, INTELLECTUAL PROPERTY RIGHTS, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
Definition in file DC570A.ino.
Go to the source code of this file.
Functions | |
| static void | print_title () |
| Prints the title block when program first starts. More... | |
| static void | print_prompt () |
| Prints main menu. More... | |
| static void | print_user_command (uint8_t menu) |
| static void | menu_1_read_differential () |
| Read channels in differential mode. More... | |
| static void | menu_2_set_OSR () |
| static void | setup () |
| Initialize Linduino. More... | |
| static void | loop () |
| Repeats Linduino loop. More... | |
| static void | menu_set_OSR () |
| Set the OSR. More... | |
Variables | |
| static uint8_t | demo_board_connected |
| Set to 1 if the board is connected. More... | |
| static int16_t | OSR_mode = LTC2440_OSR_32768 |
| The LTC2440 OSR mode settings. More... | |
| static float | LTC2440_vref = 5.0 |
|
static |
Repeats Linduino loop.
Definition at line 123 of file DC570A.ino.
|
static |
Read channels in differential mode.
Definition at line 178 of file DC570A.ino.
|
static |
|
static |
Set the OSR.
Definition at line 212 of file DC570A.ino.
|
static |
Prints main menu.
Definition at line 169 of file DC570A.ino.
|
static |
Prints the title block when program first starts.
Definition at line 154 of file DC570A.ino.
|
static |
|
static |
Initialize Linduino.
Definition at line 100 of file DC570A.ino.
|
static |
Set to 1 if the board is connected.
Definition at line 95 of file DC570A.ino.
|
static |
Definition at line 97 of file DC570A.ino.
|
static |
The LTC2440 OSR mode settings.
Definition at line 96 of file DC570A.ino.