![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
Analog Devices DC2839A Demonstration Board. More...
Analog Devices DC2839A Demonstration Board.
LTC6115: High Voltage High Side Current and Voltage Sense.
NOTES Setup: Set the terminal baud rate to 115200 and select the newline terminator. Equipment required is a voltage source (preferably low-noise) and a precision voltmeter. Ensure all jumpers on the demo board are installed in their default positions from the factory. Refer to Demo Manual for LTC6115. How to test: The voltage source should be connected to input AIN+/AIN-. Ensure the input is within its specified absolute input voltage range. (It is easiest to tie the voltage source negative terminal to COM.) Ensure the voltage source is set within the range of 0V to +5.00V. USER INPUT DATA FORMAT: decimal : 1024 hex : 0x400 octal : 02000 (leading 0 "zero") binary : B10000000000 float : 1024.0
https://www.analog.com/en/products/ltc6115.html
Copyright (c) 2018, Analog Devices Inc. (ADI) All rights reserved.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
The views and conclusions contained in the software and documentation are those of the authors and should not be interpreted as representing official policies, either expressed or implied, of Analog Devices Inc.
The Analog Devices Linduino is not affiliated with the official Arduino team. However, the Linduino is only possible because of the Arduino team's commitment to the open-source community. Please, visit http://www.arduino.cc and http://store.arduino.cc , and consider a purchase that will help fund their ongoing work.
Definition in file DC2839A.ino.
Go to the source code of this file.
Functions | |
| static void | print_title () |
| Prints the title block when program first starts. More... | |
| static void | print_prompt () |
| Prints main menu. More... | |
| static void | setup () |
| Initialize Linduino. More... | |
| static void | loop () |
| Repeats Linduino loop. More... | |
| static float | menu_1_convert_read () |
| Read channel. More... | |
| static void | menu_2_changeVGain () |
| static void | menu_3_changeIGain () |
| Select current channel transimpedance gain (V/A) More... | |
| static void | menu_4_changeSampleFreq () |
| Changes the sampling frequency (ms) More... | |
| static void | update_compare_reg (uint32_t regVal) |
| Updates the compare match register. More... | |
| static void | menu_5_pipeToFile () |
| Pipes voltage and current reading results to a file. More... | |
| static void | menu_6_stopSampling () |
| Stops the sampling from menu 5. More... | |
| ISR (TIMER1_COMPA_vect) | |
| Timer Compare Interrupt Service Routine. More... | |
Macros | |
| #define | LTC6115_GPIO QUIKEVAL_GPIO |
| Linduino QuikEval GPIO pin (QuikEval connector pin 14) connects to Arduino pin 9. More... | |
Variables | |
| volatile float | start_millis |
| Start time when menu 4 function is called. More... | |
| volatile float | current_millis |
| Number of elapsed milliseconds since the program started running. More... | |
| volatile float | globaltime_ms |
| Number of elapsed milliseconds since menu 4 function is called. More... | |
| volatile int | ISR_flag |
| Set to 1 when interrupt service routine is running. More... | |
| volatile int | samples_counter |
| Counts the number of samples taken. More... | |
| volatile int | num_samples |
| Total number of samples that the user desires. More... | |
| static int | update_interval |
| Sampling interval(ms) to update to. More... | |
| static int | compare_reg |
| Value to set compare match register to get desired interrupt frequency (Hz) More... | |
| volatile int | print_flag |
| Set to 1 to print sampling data for menu option 4. More... | |
| volatile int | ISR_prompt_flag |
| Set to 1 to print prompt after interrupt service completes. More... | |
| volatile uint32_t | readV |
| Stores voltage reading. More... | |
| volatile uint32_t | readI |
| Stores current reading. More... | |
| ISR | ( | TIMER1_COMPA_vect | ) |
Timer Compare Interrupt Service Routine.
Definition at line 396 of file DC2839A.ino.
|
static |
|
static |
|
static |
Definition at line 289 of file DC2839A.ino.
|
static |
Select current channel transimpedance gain (V/A)
Definition at line 311 of file DC2839A.ino.
|
static |
|
static |
Pipes voltage and current reading results to a file.
Definition at line 370 of file DC2839A.ino.
|
static |
|
static |
|
static |
Prints the title block when program first starts.
Definition at line 432 of file DC2839A.ino.
|
static |
|
static |
| #define LTC6115_GPIO QUIKEVAL_GPIO |
Linduino QuikEval GPIO pin (QuikEval connector pin 14) connects to Arduino pin 9.
Definition at line 82 of file DC2839A.ino.
|
static |
Value to set compare match register to get desired interrupt frequency (Hz)
Definition at line 99 of file DC2839A.ino.
| volatile float current_millis |
Number of elapsed milliseconds since the program started running.
Definition at line 93 of file DC2839A.ino.
| volatile float globaltime_ms |
Number of elapsed milliseconds since menu 4 function is called.
Definition at line 94 of file DC2839A.ino.
| volatile int ISR_flag |
Set to 1 when interrupt service routine is running.
Definition at line 95 of file DC2839A.ino.
| volatile int ISR_prompt_flag |
Set to 1 to print prompt after interrupt service completes.
Definition at line 101 of file DC2839A.ino.
| volatile int num_samples |
Total number of samples that the user desires.
Definition at line 97 of file DC2839A.ino.
| volatile int print_flag |
Set to 1 to print sampling data for menu option 4.
Definition at line 100 of file DC2839A.ino.
| volatile uint32_t readI |
Stores current reading.
Definition at line 103 of file DC2839A.ino.
| volatile uint32_t readV |
Stores voltage reading.
Definition at line 102 of file DC2839A.ino.
| volatile int samples_counter |
Counts the number of samples taken.
Definition at line 96 of file DC2839A.ino.
| volatile float start_millis |
Start time when menu 4 function is called.
Definition at line 92 of file DC2839A.ino.
|
static |
Sampling interval(ms) to update to.
Definition at line 98 of file DC2839A.ino.