![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
Linear Technology DC2091A Demonstration Board. More...
Linear Technology DC2091A Demonstration Board.
LTC5599: 130 to 1300MHz IQ Modulator.
NOTES Setup: Set the terminal baud rate to 115200 and select the newline terminator. USER INPUT DATA FORMAT: decimal : 1024 hex : 0x400 octal : 02000 (leading 0 "zero") binary : B10000000000 float : 1024.0
http://www.linear.com/product/LTC5599
http://www.linear.com/product/LTC5599#demoboards
Copyright 2018(c) Analog Devices, Inc.
All rights reserved.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
THIS SOFTWARE IS PROVIDED BY ANALOG DEVICES "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, NON-INFRINGEMENT, MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL ANALOG DEVICES BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, INTELLECTUAL PROPERTY RIGHTS, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
Definition in file DC2091A.ino.
Go to the source code of this file.
Functions | |
| static void | print_title () |
| Prints the title block when program first starts. More... | |
| static void | print_prompt () |
| Prints main menu. More... | |
| static void | print_user_command (uint8_t menu) |
| static void | menu_1_read_register () |
| Read register @ return void. More... | |
| static void | menu_2_write_register () |
| Write to register & readback @ return void. More... | |
| static void | setup () |
| Initialize Linduino. More... | |
| static void | loop () |
| Repeats Linduino loop. More... | |
Variables | |
| static uint8_t | address |
| static uint8_t | rw |
|
static |
Repeats Linduino loop.
Definition at line 100 of file DC2091A.ino.
|
static |
Read register @ return void.
Definition at line 130 of file DC2091A.ino.
|
static |
Write to register & readback @ return void.
Definition at line 155 of file DC2091A.ino.
|
static |
Prints main menu.
Definition at line 203 of file DC2091A.ino.
|
static |
Prints the title block when program first starts.
Definition at line 187 of file DC2091A.ino.
|
static |
|
static |
Initialize Linduino.
Definition at line 87 of file DC2091A.ino.
|
static |
Definition at line 83 of file DC2091A.ino.
|
static |
Definition at line 84 of file DC2091A.ino.