![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
Go to the source code of this file.
Functions | |
| static int8_t | menu_1_read_write_registers () |
| Linear Technology DC1976A Demonstration Board LTC3676: Power Management Solution for Application Processors. More... | |
| static int8_t | menu_2_regulator_settings () |
| static int8_t | menu_3_control_settings () |
| static int8_t | menu_4_sequencing (uint8_t *reg_phase) |
| static void | print_title () |
| Prints the title block when program first starts. More... | |
| static void | print_prompt () |
| Prints main menu. More... | |
| static void | print_warning_prompt () |
| Prints a warning if the demo board is not detected. More... | |
| static int8_t | LTC3676_print_all_registers (uint8_t i2c_address) |
| static void | read_reg_map (uint8_t *reg_map_array) |
| Reads the first 6 registers and stores them in an array. More... | |
| static void | setup () |
| Initialize Linduino. More... | |
| static void | loop () |
| Repeats Linduino loop. More... | |
| char | demo_board_option (char *eeprom_string) |
Variables | |
| static uint8_t | demo_board_connected |
| Set to 1 if the board is connected. More... | |
| static uint8_t | i2c_address |
| I2C address set for either -A or -B demo board. More... | |
| static char | board_option |
| Demo board option of the attached demo board. More... | |
| char | demo_name [] = "DC1976" |
| Demo Board Name stored in QuikEval EEPROM. More... | |
| static uint8_t | reg_phase [7] = {1,1,1,1,1,1,1} |
| Power-up sequence phases for every regulator output. More... | |
| static float | delay_ms = 0 |
| Delay between power-up phases. More... | |
| char demo_board_option | ( | char * | eeprom_string | ) |
Definition at line 200 of file DC1976A.ino.
|
static |
Repeats Linduino loop.
Definition at line 110 of file DC1976A.ino.
|
static |
Definition at line 182 of file DC1976A.ino.
|
static |
Linear Technology DC1976A Demonstration Board LTC3676: Power Management Solution for Application Processors.
NOTES Setup: Set the terminal baud rate to 115200 and select the newline terminator. External power supply is required. Any assembly option may be used: DC1976A-A, DC1976A-B.
http://www.linear.com/product/LTC3676
http://www.linear.com/product/LTC3676#demoboards
Copyright 2018(c) Analog Devices, Inc.
All rights reserved.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
THIS SOFTWARE IS PROVIDED BY ANALOG DEVICES "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, NON-INFRINGEMENT, MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL ANALOG DEVICES BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, INTELLECTUAL PROPERTY RIGHTS, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
Definition at line 212 of file DC1976A.ino.
|
static |
Definition at line 363 of file DC1976A.ino.
|
static |
Definition at line 704 of file DC1976A.ino.
|
static |
Definition at line 772 of file DC1976A.ino.
|
static |
Prints main menu.
Definition at line 167 of file DC1976A.ino.
|
static |
Prints the title block when program first starts.
Definition at line 152 of file DC1976A.ino.
|
static |
Prints a warning if the demo board is not detected.
Definition at line 177 of file DC1976A.ino.
|
static |
Reads the first 6 registers and stores them in an array.
Definition at line 1015 of file DC1976A.ino.
|
static |
Initialize Linduino.
Definition at line 83 of file DC1976A.ino.
|
static |
Demo board option of the attached demo board.
Definition at line 77 of file DC1976A.ino.
|
static |
Delay between power-up phases.
Definition at line 80 of file DC1976A.ino.
|
static |
Set to 1 if the board is connected.
Definition at line 75 of file DC1976A.ino.
| char demo_name[] = "DC1976" |
Demo Board Name stored in QuikEval EEPROM.
Definition at line 78 of file DC1976A.ino.
|
static |
I2C address set for either -A or -B demo board.
Definition at line 76 of file DC1976A.ino.
|
static |
Power-up sequence phases for every regulator output.
Definition at line 79 of file DC1976A.ino.