![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
Linear Technology DC1785 Demonstration Board. More...
Linear Technology DC1785 Demonstration Board.
LTC2991: 14-bit ADC Octal I2C Voltage, Current, and Temperature monitor.
Setup:
Set the terminal baud rate to 115200 and select the newline terminator.
A precision voltage source (preferably low-noise) may be used to apply a voltage
to input terminals V1-V8. A precision voltmeter may be used to verify applied
voltages. An oscilloscope may be used to view the PWM output. Ensure JP5, JP6
and JP7 are in the LOW position. Refer to Demo Manual DC1785A
Explanation of Commands:
1 - Single-Ended Voltage - Selects the Single-Ended Voltage Menu.
1-8: Displays the measured single-ended voltage at one of the V1-V8
inputs. When measuring V1 and V8, ensure jumpers are set to VOLT
position.
9: Vcc - Displays the measured Vcc voltage.
10: ALL - Displays the measured voltages at all of the V1-V8 inputs
and Vcc.
2 - Differential Voltage - Selects the Differential Voltage Menu.
Maximum full scale differential voltage is 0.300V.
1-4: Displays the measured differential voltage across one of the V1-V8
input pairs. The input common-mode range is 0V to Vcc. It is
easiest to ground the lower input. When measuring V1 and V8,
ensure jumpers are set to VOLT position.
5: ALL - Displays the measured differential voltages at all terminals.
3 - Temperature - Selects the Temperature Menu
To measure temperature using onboard transistors, set JP1, JP2, JP3 and JP4
to TEMP position.
1: V1-V2 - Measure temperature of Q1 (mounted to demo board) when JP1
and JP2 are in TEMP position.
2: V3-V4 - Measure temperature of external transistor connected to V3
and V4 terminals.
3: V5-V6 - Measure temperature of external transistor connected to V5
and V6 terminals.
4: V7-V8 - Measure temperature of Q2 (mounted to demo board) when JP3
and JP4 are in TEMP position.
5: Internal - Measure temperature using the internal temperature
sensor.
6: All - Displays temperatures at all connections as well as the
internal temperature sensor.
4 - Settings - Selects the Settings Menu
Enable/disable the on-chip digital filters. Also toggle temperature units
between degrees Celsius or degrees Kelvin.
1-5: Entering these one can enable/disable various channel filters.
6: Toggle temperature units between degrees Celsius and degrees
Kelvin.
5 - PWM - Selects the PWM Menu
Generates Proportional PWM output using remote diode connected to pins 7 and
8. When JP3 and JP4 are in TEMP positions, Q2 is used as the temperature
sensing diode (mounted on demo board).
1: Set Threshold Temperature - Enter temperature corresponding to 0%
(100% in Inverted Mode) duty cycle.
2: Inverted/Non-Inverted PWM - Toggles between Inverted/Non-Inverted
modes
3: Enable/Disable - Enables or Disables PWM (Toggle)
USER INPUT DATA FORMAT:
decimal : 1024
hex : 0x400
octal : 02000 (leading 0 "zero")
binary : B10000000000
float : 1024.0http://www.linear.com/product/LTC2991
http://www.linear.com/product/LTC2991#demoboards
Copyright 2018(c) Analog Devices, Inc.
All rights reserved.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
THIS SOFTWARE IS PROVIDED BY ANALOG DEVICES "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, NON-INFRINGEMENT, MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL ANALOG DEVICES BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, INTELLECTUAL PROPERTY RIGHTS, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
Definition in file DC1785A.ino.
Go to the source code of this file.
Functions | |
| static void | print_title () |
| Prints the title block when program first starts. More... | |
| static void | print_prompt () |
| Prints main menu. More... | |
| static int8_t | menu_1_single_ended_voltage () |
| Read single-ended voltages. More... | |
| static int8_t | menu_2_read_differential_voltage () |
| Read differential voltages. More... | |
| static int8_t | menu_3_read_temperature () |
| Read temperatures. More... | |
| static int8_t | menu_4_settings () |
| Configure settings. More... | |
| static int8_t | menu_5_pwm_options () |
| Configure PWM options. More... | |
| static void | setup () |
| Initialize Linduino. More... | |
| static void | loop () |
| Repeats Linduino loop. More... | |
Variables | |
| static uint8_t | demo_board_connected |
| Set to 1 if the board is connected. More... | |
| const uint16_t | LTC2991_TIMEOUT =1000 |
| Configures the maximum timeout allowed for an LTC2991 read. More... | |
|
static |
Repeats Linduino loop.
Definition at line 164 of file DC1785A.ino.
|
static |
Read single-ended voltages.
Definition at line 237 of file DC1785A.ino.
|
static |
Read differential voltages.
Definition at line 446 of file DC1785A.ino.
|
static |
Read temperatures.
Definition at line 564 of file DC1785A.ino.
|
static |
Configure settings.
Definition at line 764 of file DC1785A.ino.
|
static |
Configure PWM options.
Definition at line 871 of file DC1785A.ino.
|
static |
Prints main menu.
Definition at line 225 of file DC1785A.ino.
|
static |
Prints the title block when program first starts.
Definition at line 210 of file DC1785A.ino.
|
static |
Initialize Linduino.
Definition at line 144 of file DC1785A.ino.
|
static |
Set to 1 if the board is connected.
Definition at line 139 of file DC1785A.ino.
| const uint16_t LTC2991_TIMEOUT =1000 |
Configures the maximum timeout allowed for an LTC2991 read.
Definition at line 141 of file DC1785A.ino.