![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
LTC4155: Dual-Input Power Manager / 3.5A Li-Ion Battery Charger with I²C Control and USB OTG. More...
LTC4155: Dual-Input Power Manager / 3.5A Li-Ion Battery Charger with I²C Control and USB OTG.
The LTC®4155 is a 15 watt I²C controlled power manager with PowerPath™ instant- on operation, high efficiency switching battery charging and USB compatibility. The LTC4155 seamlessly manages power distribution from two 5V sources, such as a USB port and a wall adapter, to a single-cell rechargeable Lithium-Ion/Polymer battery and a system load.
http://www.linear.com/product/LTC4155
http://www.linear.com/product/LTC4155#demoboards
Copyright 2018(c) Analog Devices, Inc.
All rights reserved.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
THIS SOFTWARE IS PROVIDED BY ANALOG DEVICES "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, NON-INFRINGEMENT, MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL ANALOG DEVICES BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, INTELLECTUAL PROPERTY RIGHTS, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
Generated on: 2016-01-19
Arduino Example
This is an example sketch to demonstrate use of the API with the Linduino. In addition to the sketch, the following files are required:: LTC4155.c LTC4155.h LTC4155_reg_defs.h
Definition in file DC1674A.ino.
Go to the source code of this file.
Functions | |
| static int | read_register (uint8_t addr, uint8_t command_code, uint8_t *data, port_configuration_t *port_configuration) |
| read_register function wraps C++ method LT_SMBus::readByte and places the returned data in *data. More... | |
| static int | write_register (uint8_t addr, uint8_t command_code, uint8_t data, port_configuration_t *port_configuration) |
| write_register function wraps C++ method LT_SMBus::writeByte. More... | |
| static void | setup () |
| static void | loop () |
Variables | |
| static LT_SMBus * | smbus = new LT_SMBusNoPec() |
| LTC4155_chip_cfg_t | cfg |
| LTC4155 | chip |
| static uint8_t | data |
|
static |
Definition at line 99 of file DC1674A.ino.
|
static |
read_register function wraps C++ method LT_SMBus::readByte and places the returned data in *data.
Definition at line 119 of file DC1674A.ino.
|
static |
Definition at line 91 of file DC1674A.ino.
|
static |
write_register function wraps C++ method LT_SMBus::writeByte.
Definition at line 127 of file DC1674A.ino.
Definition at line 79 of file DC1674A.ino.
| LTC4155 chip |
Definition at line 88 of file DC1674A.ino.
|
static |
Definition at line 89 of file DC1674A.ino.
|
static |
Definition at line 74 of file DC1674A.ino.