![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
Linear Technology DC1490A-A Demonstration Board. More...
Linear Technology DC1490A-A Demonstration Board.
LTC2460: 24-Bit, 16-Channel Delta Sigma ADC with SPI interface
NOTES Setup: Set the terminal baud rate to 115200 and select the newline terminator. Equipment required is a precision voltage source and a precision voltmeter. Additionally, an external power supply is required to provide a negative voltage for Amp V-. Set it to anywhere from -1V to -5V. Set Amp V+ to Vcc. Ensure the COM and REF- pins are connected to ground. The REF+ pin should be connected to +5V. How to test Single-Ended mode: The voltage source should be connected to the ADC such that the negative lead is connected to the COM(common) pin. The positive lead may be connected to any channel input. Ensure voltage is within analog input voltage range -0.3 to 2.5V. How to test Differential Mode: The voltage source should be connected with positive and negative leads to paired channels. The voltage source negative output must also be connected to the COM pin in order to provide a ground-referenced voltage. Ensure voltage is within analog input voltage range -0.3V to +2.5V. Swapping input voltages results in a reversed polarity reading. How to calibrate: Apply 100mV CH0 with respect to COM. Next, measure this voltage with a precise voltmeter and enter this value. (This takes the reading.) Now apply approximately 2.40 volts to CH0. Measure this voltage with a precise voltmeter and enter this value. Calibration is now stored in EEPROM. Upon start-up the calibration values will be restored. USER INPUT DATA FORMAT: decimal : 1024 hex : 0x400 octal : 02000 (leading 0 "zero") binary : B10000000000 float : 1024.0
http://www.linear.com/product/LTC2460
http://www.linear.com/product/LTC2460#demoboards
Copyright 2018(c) Analog Devices, Inc.
All rights reserved.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
THIS SOFTWARE IS PROVIDED BY ANALOG DEVICES "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, NON-INFRINGEMENT, MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL ANALOG DEVICES BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, INTELLECTUAL PROPERTY RIGHTS, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
Definition in file DC1490.ino.
Go to the source code of this file.
Functions | |
| static void | print_title () |
| Prints the title block when program first starts. More... | |
| static void | print_prompt () |
| Prints main menu. More... | |
| static void | menu_1_read_single_ended () |
| Read channels in single-ended mode. More... | |
| static void | menu_2_set_1X2X () |
| Set 1X or 2X mode. More... | |
| static void | setup () |
| Initialize Linduino. More... | |
| static void | loop () |
| Repeats Linduino loop. More... | |
| static void | menu_3_sleep () |
Variables | |
| static uint8_t | demo_board_connected |
| Set to 1 if the board is connected. More... | |
| static int16_t | two_x_mode = LTC2460_SPEED_1X |
| The LTC2460 2X Mode settings. More... | |
| static float | LTC2460_vref = 1.25 |
| static uint16_t | eoc_timeout = 25 |
| const uint16_t | BUILD_1X_2X_COMMAND [2] = {LTC2460_SPEED_1X, LTC2460_SPEED_2X} |
| Lookup table to build 1X / 2X bits. More... | |
|
static |
Repeats Linduino loop.
Definition at line 141 of file DC1490.ino.
|
static |
Read channels in single-ended mode.
Definition at line 199 of file DC1490.ino.
|
static |
Set 1X or 2X mode.
Definition at line 251 of file DC1490.ino.
|
static |
Definition at line 275 of file DC1490.ino.
|
static |
Prints main menu.
Definition at line 190 of file DC1490.ino.
|
static |
Prints the title block when program first starts.
Definition at line 175 of file DC1490.ino.
|
static |
Initialize Linduino.
Definition at line 117 of file DC1490.ino.
| const uint16_t BUILD_1X_2X_COMMAND[2] = {LTC2460_SPEED_1X, LTC2460_SPEED_2X} |
Lookup table to build 1X / 2X bits.
Build the command for 1x or 2x mode
Definition at line 113 of file DC1490.ino.
|
static |
Set to 1 if the board is connected.
Definition at line 106 of file DC1490.ino.
|
static |
Definition at line 109 of file DC1490.ino.
|
static |
Definition at line 108 of file DC1490.ino.
|
static |
The LTC2460 2X Mode settings.
Definition at line 107 of file DC1490.ino.