![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
Linear Technology DC1337A Demonstration Board. More...
Linear Technology DC1337A Demonstration Board.
LTC2301: 1-Channel, 12-Bit SAR ADC with I2C Interface. LTC2305: 2-Channel, 12-Bit SAR ADC with I2C Interface.
NOTES
Setup:
Set the terminal baud rate to 115200 and select the newline terminator. Equipment
required is a voltage source (preferably low-noise) and a precision voltmeter.
Ensure all jumpers on the demo board are installed in their default positions
from the factory. Refer to Demo Manual DC1444A.
LTC2301
How to test Differential Mode:
Bipolar Mode:
The voltage source should be connected between inputs VIN+ and VIN-. Ensure both
inputs are within their specified absolute input voltage range. (It is easiest
to tie the voltage source negative terminal to COM.) Ensure the voltage
source is set within the range of 0V to +4.096V (differential voltage range).
(Swapping input voltages results in a reversed polarity reading.)
Unipolar Mode:
The voltage source should be connected between inputs VIN+ and VIN-. Ensure both
inputs are within their specified absolute input voltage range. (It is easiest
to tie the voltage source negative terminal to COM.) Ensure the voltage
source is set within the range of 0V to +4.096V (differential voltage range).
LTC2305
How to test Single-Ended mode:
Bipolar Mode:
The voltage source should be connected to input VCH0 or VCH1. Ensure the input is
within its specified absolute input voltage range. (It is easiest
to tie the voltage source negative terminal to COM.) Ensure the voltage
source is set within the range of 0V to +4.096V.
(Swapping input voltages results in a reversed polarity reading.)
Unipolar Mode:
The voltage source should be connected to input VCH0 or VCH1. Ensure the input is
within its specified absolute input voltage range. (It is easiest
to tie the voltage source negative terminal to COM.) Ensure the voltage
source is set within the range of 0V to +4.096V.
USER INPUT DATA FORMAT:
decimal : 1024
hex : 0x400
octal : 02000 (leading 0 "zero")
binary : B10000000000
float : 1024.0http://www.linear.com/product/LTC2301 http://www.linear.com/product/LTC2305
http://www.linear.com/product/LTC2301#demoboards http://www.linear.com/product/LTC2305#demoboards
Copyright 2018(c) Analog Devices, Inc.
All rights reserved.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
THIS SOFTWARE IS PROVIDED BY ANALOG DEVICES "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, NON-INFRINGEMENT, MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL ANALOG DEVICES BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, INTELLECTUAL PROPERTY RIGHTS, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
Definition in file DC1444A.ino.
Go to the source code of this file.
Functions | |
| static void | print_title () |
| Prints the title block when the program first starts. More... | |
| static void | print_prompt () |
| Prints main menu. More... | |
| static uint8_t | print_user_command_single_ended () |
| Display selected single-ended channels. More... | |
| static int8_t | menu_1_read_input () |
| Read channels in single-ended mode. More... | |
| static void | menu_2_select_part () |
| Sets LTC2305 to Single-Ended or Differential. More... | |
| static void | menu_3_select_uni_bipolar () |
| Sets LTC230X to Bipolar or Unipolar. More... | |
| static void | menu_4_select_single_ended_differential () |
| Sets LTC2305 single-ended or differential mode. More... | |
| static void | menu_5_select_polarity () |
| Sets LTC2305 polarity in differential mode. More... | |
| static int8_t | menu_6_sleep () |
| Sets LTC2305 Sleep Mode. More... | |
| static void | menu_7_set_address () |
| Set the I2C 7 bit address. More... | |
| static void | setup () |
| Initialize Linduino. More... | |
| static void | loop () |
| Repeats Linduino loop. More... | |
Variables | |
| static uint8_t | demo_board_connected |
| Set to 1 if the board is connected. More... | |
| static uint8_t | single_ended_differential = LTC2305_SINGLE_ENDED_MODE |
| LTC2305 Single-Ended or Differential mode selection. More... | |
| static uint8_t | uni_bipolar = LTC2305_UNIPOLAR_MODE |
| LTC2305 Unipolar or Bipolar mode selection. More... | |
| static uint8_t | part = LTC2301 |
| LTC2301 or 2305 part selection. More... | |
| static uint8_t | polarity = LTC2305_P0_N1 |
| LTC230X Input polarity selection. More... | |
| static uint8_t | channel = LTC2305_CH0 |
| LTC2305 Channel selection. More... | |
| static uint8_t | i2c_address = LTC2305_I2C_ADDRESS |
| I2C address in 7 bit format for part. More... | |
| static uint8_t | LTC2305_bits = 12 |
| Resolution (12 bits) More... | |
| static float | LTC2305_vref = 4.096 |
| const uint8_t | BUILD_COMMAND_SINGLE_ENDED [2] = {LTC2305_CH0, LTC2305_CH1} |
| Builds the command for single-ended mode. More... | |
|
static |
Repeats Linduino loop.
Definition at line 148 of file DC1444A.ino.
|
static |
Read channels in single-ended mode.
Definition at line 197 of file DC1444A.ino.
|
static |
Sets LTC2305 to Single-Ended or Differential.
Definition at line 330 of file DC1444A.ino.
|
static |
Sets LTC230X to Bipolar or Unipolar.
Definition at line 361 of file DC1444A.ino.
|
static |
Sets LTC2305 single-ended or differential mode.
Definition at line 392 of file DC1444A.ino.
|
static |
Sets LTC2305 polarity in differential mode.
Definition at line 424 of file DC1444A.ino.
|
static |
Sets LTC2305 Sleep Mode.
Definition at line 456 of file DC1444A.ino.
|
static |
Set the I2C 7 bit address.
Definition at line 478 of file DC1444A.ino.
|
static |
Prints main menu.
Definition at line 508 of file DC1444A.ino.
|
static |
Prints the title block when the program first starts.
Definition at line 490 of file DC1444A.ino.
|
static |
Display selected single-ended channels.
Definition at line 523 of file DC1444A.ino.
|
static |
Initialize Linduino.
Definition at line 137 of file DC1444A.ino.
| const uint8_t BUILD_COMMAND_SINGLE_ENDED[2] = {LTC2305_CH0, LTC2305_CH1} |
Builds the command for single-ended mode.
Definition at line 134 of file DC1444A.ino.
|
static |
LTC2305 Channel selection.
Definition at line 127 of file DC1444A.ino.
|
static |
Set to 1 if the board is connected.
Definition at line 122 of file DC1444A.ino.
|
static |
I2C address in 7 bit format for part.
Definition at line 128 of file DC1444A.ino.
|
static |
Resolution (12 bits)
Definition at line 129 of file DC1444A.ino.
|
static |
Definition at line 130 of file DC1444A.ino.
|
static |
LTC2301 or 2305 part selection.
Definition at line 125 of file DC1444A.ino.
|
static |
LTC230X Input polarity selection.
Definition at line 126 of file DC1444A.ino.
|
static |
LTC2305 Single-Ended or Differential mode selection.
Definition at line 123 of file DC1444A.ino.
|
static |
LTC2305 Unipolar or Bipolar mode selection.
Definition at line 124 of file DC1444A.ino.