![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
Linear Technology DC1337A Demonstration Board. More...
Linear Technology DC1337A Demonstration Board.
LTC2309: 8-Channel, 12-Bit SAR ADC with I2C Interface.
Linear Technology DC1444A Demonstration Board. LTC2301: 1-Channel, 12-Bit ADCs with I2C Compatible Interface
NOTES
Setup:
Set the terminal baud rate to 115200 and select the newline terminator. Equipment
required is a voltage source (preferably low-noise) and a precision voltmeter. No
external power supply is required. Ensure all jumpers on the demo board are
installed in their default positions from the factory. Refer to Demo Manual
DC1337A.
How to test Single-Ended mode:
Bipolar Mode:
The voltage source should be connected to one of the inputs CH0,...CH7. Ensure the input is
within its specified absolute input voltage range. (It is easiest
to tie the voltage source negative terminal to COM.) Ensure the voltage
source is set within the range of 0V to +4.096V.
(Swapping input voltages results in a reversed polarity reading.)
Unipolar Mode:
The voltage source should be connected to one of the inputs CH0,...CH7. Ensure the input is
within its specified absolute input voltage range. (It is easiest
to tie the voltage source negative terminal to COM.) Ensure the voltage
source is set within the range of 0V to +4.096V.
How to test Differential Mode:
Bipolar Mode:
The voltage source should be connected between paired channels. Ensure both
inputs are within their specified absolute input voltage range. (It is easiest
to tie the voltage source negative terminal to COM or GND.) Ensure the voltage
source is set within the range of 0 to +4.096V (differential voltage range).
(Swapping input voltages results in a reversed polarity reading.)
Unipolar Mode:
The voltage source should be connected between paired channels. (It is easiest
to tie the voltage source negative terminal to COM or GND.) Ensure both inputs
are within their specified absolute input voltage range. (It is easiest to tie
the voltage source negative terminal to COM or GND.) Ensure the voltage source
is set within the range of 0 to +4.096V (differential voltage range).
USER INPUT DATA FORMAT:
decimal : 1024
hex : 0x400
octal : 02000 (leading 0 "zero")
binary : B10000000000
float : 1024.0http://www.linear.com/product/LTC2309 http://www.linear.com/product/LTC2301
http://www.linear.com/product/LTC2309#demoboards http://www.linear.com/product/LTC2301#demoboards
Copyright 2018(c) Analog Devices, Inc.
All rights reserved.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
THIS SOFTWARE IS PROVIDED BY ANALOG DEVICES "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, NON-INFRINGEMENT, MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL ANALOG DEVICES BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, INTELLECTUAL PROPERTY RIGHTS, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
Definition in file DC1337A.ino.
Go to the source code of this file.
Functions | |
| static void | print_title () |
| Prints the title block when the program first starts. More... | |
| static void | print_prompt () |
| Prints main menu. More... | |
| static uint8_t | print_user_command_differential () |
| Display selected differential channels. More... | |
| static uint8_t | print_user_command_single_ended () |
| Display selected differential channels. More... | |
| static void | print_channel_selection (uint8_t menu) |
| Display selected differential channels. More... | |
| static int8_t | menu_1_read_input () |
| Read channels. More... | |
| static void | menu_3_select_uni_bipolar () |
| Sets LTC2309 to Bipolar or Unipolar. More... | |
| static void | menu_2_select_single_ended_differential () |
| Sets LTC2309 to Single-Ended or Differential. More... | |
| static int8_t | menu_4_sleep () |
| static void | menu_5_set_address () |
| static void | setup () |
| Initialize Linduino. More... | |
| static void | loop () |
| Repeats Linduino loop. More... | |
| static void | menu_4_set_address () |
| Set the I2C 7 bit address. More... | |
| static int8_t | menu_5_sleep () |
| Sets LTC2309 Sleep Mode. More... | |
Variables | |
| static uint8_t | uni_bipolar = LTC2309_UNIPOLAR_MODE |
| LTC2309 Unipolar or Bipolar mode selection. More... | |
| static uint8_t | single_ended_differential = LTC2309_SINGLE_ENDED_MODE |
| LTC2309 Unipolar or Bipolar mode selection. More... | |
| static uint8_t | i2c_address = LTC2309_I2C_ADDRESS |
| I2C address in 7 bit format for part. More... | |
| static uint8_t | LTC2309_bits = 12 |
| Resolution (12 bits) More... | |
| static float | LTC2309_vref = 4.096 |
| const uint8_t | BUILD_COMMAND_SINGLE_ENDED [8] |
| Builds the command for single-ended mode. More... | |
| const uint8_t | BUILD_COMMAND_DIFF [8] |
| Build the command for differential mode. More... | |
|
static |
Repeats Linduino loop.
Definition at line 151 of file DC1337A.ino.
|
static |
|
static |
Sets LTC2309 to Single-Ended or Differential.
Definition at line 294 of file DC1337A.ino.
|
static |
Sets LTC2309 to Bipolar or Unipolar.
Definition at line 325 of file DC1337A.ino.
|
static |
Set the I2C 7 bit address.
Definition at line 356 of file DC1337A.ino.
|
static |
|
static |
|
static |
Sets LTC2309 Sleep Mode.
Definition at line 369 of file DC1337A.ino.
|
static |
Display selected differential channels.
Displaying single-ended channels is straightforward; not so with differential because the inputs can take either polarity.
Definition at line 477 of file DC1337A.ino.
|
static |
Prints main menu.
Definition at line 406 of file DC1337A.ino.
|
static |
Prints the title block when the program first starts.
Definition at line 391 of file DC1337A.ino.
|
static |
Display selected differential channels.
Displaying single-ended channels is straightforward; not so with differential because the inputs can take either polarity.
Definition at line 419 of file DC1337A.ino.
|
static |
Display selected differential channels.
Displaying single-ended channels is straightforward; not so with differential because the inputs can take either polarity.
Definition at line 511 of file DC1337A.ino.
|
static |
Initialize Linduino.
Definition at line 141 of file DC1337A.ino.
| const uint8_t BUILD_COMMAND_DIFF[8] |
Build the command for differential mode.
Definition at line 136 of file DC1337A.ino.
| const uint8_t BUILD_COMMAND_SINGLE_ENDED[8] |
Builds the command for single-ended mode.
Definition at line 132 of file DC1337A.ino.
|
static |
I2C address in 7 bit format for part.
Definition at line 126 of file DC1337A.ino.
|
static |
Resolution (12 bits)
Definition at line 127 of file DC1337A.ino.
|
static |
Definition at line 128 of file DC1337A.ino.
|
static |
LTC2309 Unipolar or Bipolar mode selection.
Definition at line 125 of file DC1337A.ino.
|
static |
LTC2309 Unipolar or Bipolar mode selection.
Definition at line 124 of file DC1337A.ino.