![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
DC1208A High Voltage I2C Current and Voltage Monitor. More...
DC1208A High Voltage I2C Current and Voltage Monitor.
Setup:
Set the terminal baud rate to 115200 and select the newline terminator. Refer
to Demo Manual DC1208A. Ensure all jumpers are installed in the factory default
positions. A power supply and load resistor are required. A DVM may be used to
verify displayed voltage results. A precision voltage source (preferably
low-noise) may be used to apply a voltage to the ADIN pin. For all tests,
connect power supply between VIN and GND, 7V-75V. Connect a load resistor to
Vout and GND.
Command Description:
*****Main Menu*****
1- Read Continuous Mode- If selected, program keeps taking readings every second
or so. In this mode, the program displays Load Current, VIN Voltage and ADIN
voltage.
2- Snapshot Mode- Selecting this option causes display of the Snapshot Mode
Menu. Readings are taken just once for each Snapshot Mode menu entry.
***** SNAPSHOT MODE MENU COMMANDS *****
1- Load Current- Selecting this option causes load current to be displayed.
2- V_IN Voltage- Selecting this option causes VIN voltage to be displayed.
3- ADIN Voltage- Selecting this option causes the voltage at the ADIN pin to
be displayed.
USER INPUT DATA FORMAT:
decimal : 1024
hex : 0x400
octal : 02000 (leading 0 "zero")
binary : B10000000000
float : 1024.0Copyright 2018(c) Analog Devices, Inc.
All rights reserved.
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
THIS SOFTWARE IS PROVIDED BY ANALOG DEVICES "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, NON-INFRINGEMENT, MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL ANALOG DEVICES BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, INTELLECTUAL PROPERTY RIGHTS, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
Definition in file DC1208A.ino.
Go to the source code of this file.
Functions | |
| static void | print_title () |
| Prints the title block when program first starts. More... | |
| static void | print_prompt () |
| Prints main menu. More... | |
| static int8_t | LTC4151_snapshot (uint8_t i2c_address, uint8_t channel) |
| Build and send the snapshot command. More... | |
| static int8_t | menu_1_continuous_mode () |
| Reads all inputs in continuous mode. More... | |
| static int8_t | menu_2_snapshot_mode () |
| Reads inputs in snapshot mode. More... | |
| static void | setup () |
| Initialize Linduino. More... | |
| static void | loop () |
| Repeats Linduino loop. More... | |
Variables | |
| static int8_t | demo_board_connected |
| Set to 1 if the board is connected. More... | |
| const float | resistor = .02 |
| Sense resistor value. More... | |
| const float | LTC4151_sense_lsb = 20e-6 |
| Typical sense lsb weight in volts. More... | |
| const float | LTC4151_vin_lsb = 25e-3 |
| Typical Vin lsb weight in volts. More... | |
| const float | LTC4151_adin_lsb = 0.5 |
| Typical ADIN lsb weight in mV. More... | |
|
static |
Repeats Linduino loop.
Definition at line 126 of file DC1208A.ino.
|
static |
Build and send the snapshot command.
| i2c_address | I2C address of the LTC4151. |
| channel | Desired channel from the header |
Definition at line 187 of file DC1208A.ino.
|
static |
Reads all inputs in continuous mode.
Definition at line 198 of file DC1208A.ino.
|
static |
Reads inputs in snapshot mode.
Definition at line 243 of file DC1208A.ino.
|
static |
Prints main menu.
Definition at line 176 of file DC1208A.ino.
|
static |
Prints the title block when program first starts.
Definition at line 162 of file DC1208A.ino.
|
static |
Initialize Linduino.
Definition at line 113 of file DC1208A.ino.
|
static |
Set to 1 if the board is connected.
Definition at line 104 of file DC1208A.ino.
| const float LTC4151_adin_lsb = 0.5 |
Typical ADIN lsb weight in mV.
Definition at line 110 of file DC1208A.ino.
| const float LTC4151_sense_lsb = 20e-6 |
Typical sense lsb weight in volts.
Definition at line 108 of file DC1208A.ino.
| const float LTC4151_vin_lsb = 25e-3 |
Typical Vin lsb weight in volts.
Definition at line 109 of file DC1208A.ino.
| const float resistor = .02 |
Sense resistor value.
Definition at line 106 of file DC1208A.ino.