![]() |
Linduino
1.3.0
Linear Technology Arduino-Compatible Demonstration Board
|
Go to the source code of this file.
Macros | |
| #define | pgm_read_byte(addr) (*(const unsigned char *)(addr)) |
| #define | pgm_read_word(addr) (*(const unsigned short *)(addr)) |
| #define | pgm_read_dword(addr) (*(const unsigned long *)(addr)) |
| #define | pgm_read_pointer(addr) ((void *)pgm_read_dword(addr)) |
| #define | min(a, b) (((a) < (b)) ? (a) : (b)) |
| #define | _swap_int16_t(a, b) { int16_t t = a; a = b; b = t; } |
| #define _swap_int16_t | ( | a, | |
| b | |||
| ) | { int16_t t = a; a = b; b = t; } |
Definition at line 70 of file Adafruit_GFX.cpp.
| #define min | ( | a, | |
| b | |||
| ) | (((a) < (b)) ? (a) : (b)) |
Definition at line 66 of file Adafruit_GFX.cpp.
| #define pgm_read_byte | ( | addr | ) | (*(const unsigned char *)(addr)) |
Definition at line 47 of file Adafruit_GFX.cpp.
| #define pgm_read_dword | ( | addr | ) | (*(const unsigned long *)(addr)) |
Definition at line 53 of file Adafruit_GFX.cpp.
| #define pgm_read_pointer | ( | addr | ) | ((void *)pgm_read_dword(addr)) |
Definition at line 60 of file Adafruit_GFX.cpp.
| #define pgm_read_word | ( | addr | ) | (*(const unsigned short *)(addr)) |
Definition at line 50 of file Adafruit_GFX.cpp.