NOISE and 5B's Noise is usually a difficult problem to overcome. The reason for the difficulty is that it is so hard to find the source. This technote should help you to isolate any noise that you may see with the 5B modules. When you can detect noise in your measurement application that is using 5B modules you should first try to isolate the problem to the transducer, signal Conditioner (5B) or measurement system. To isolate the 5B module you want to disconnect the input from your transducer and apply the appropriate input setup for each module: Module Input setup 5B30/31/40/41 Shorted 5B32 Shorted 5B34 RTD or 100 ohm resistor 5B37/47 Shorted 5B38 Excitation is balanced with any 2 equal value resistors greater than 300 ohms with the center of the resistors tied to the (-) input. Then short the (+) and (-) inputs. These setups should give a steady DC signal on the output. (Either 0 volts or offset.) The next step is to measure the output of the 5B module. And depending on the bandwidth of the measurement system you can see different results. Until recently All 5B modules showed a noise component that is from the high frequency mod-demod circuitry within the 5B module (from the transformer isolation section). This "noise" is at a frequency that is the carrier frequency of the individual 5B module. It is in the form of a very fast rise and fall time spike signal. The amplitude of this noise spike will depend upon the bandwidth of the measurement system you use. For example, if you take a lOOmHz bandwidth scope and look at the output directly of a 5B module, you may see a pk-pk amplitude of 150 mV .. but if you take a scope with a l0kHz bandwidth, and look at the same module you may see a pk-pk amplitude for this noise spike of only 5 mV. The reason for this explanation of the "change" in the apparent amplitude of the noise spike is to get back to the issue of the bandwidth of the measurement system. And why this noise will not be a problem in some applications and why it will be a problem in others. For example : if the measurement system connected to the output of a 5B module is a successive approximation type of A/D or an integrating type of A/D, this noise is not "seen" .. it is much too fast and is never a problem. However, if the measurement system is a sampling A/D system, this noise spike can be a problem because that is the type of measurement system which will "see" fast spikes. If you are using a sampling A/D system you could try placing by-pass capacitors on the outputs of the 5B modules, to by-pass this high frequency noise to ground at the output of each module. Try using 0.1 ufd capacitors. Because of the increased use of 5B modules in applications utilizing sampling A/D's, Analog devices has come up with a design change to all 5B modules to significantly reduce this high frequency spike noise at the output of each module. The new modules are specified to have a worst case noise of .6mVpk-pk @ 100KHZ bandwidth and a worst case 14mVpk-pk @ 5MHz bandwidth. These new specifications for the modules make them the best signal conditioners available on the market. Each model has undergone this change at different times. You can check the 4 digit date codes of your modules to see if the number is less than the ones listed below. All modules with the date codes below or greater have the low noise change.The date codes are as follows: Model Date Code 5B30/31/32 9316 5B40/41 9326 5B34 9327 5B37 9327 5B47 9328 Note: Please understand that we do not replace any 5B modules that are before these dates.