====================================================================== - WmSharcIce - SHARC JTAG Emulator Debug Target DLL Version 4.70.6 Analog Devices, Inc. ====================================================================== WmSharcIce is a SHARC JTAG Debug Target for VisualDSP++ 2.0, or greater. It will provide full JTAG debug support for all 2106x, 2116x, and 2126x processors using an external emulator such as the Summit-ICE or Mountain-ICE from Analog Devices. ====================================================================== Requirements ====================================================================== - VisualDSP++ 2.0, or greater with SHARC support - A Summit-ICE - Windows 98, Windows NT 4.0 with SP3 or greater, Windows 2000, Windows ME, or Windows XP. ====================================================================== Installation and Usage Notes ====================================================================== - Operation under Windows requires the proper JTAG Emulator Driver from Analog Devices, Inc. to be installed and running. The driver installation is integrated into the Emulation Tools setup for Windows NT. - After installation the JTAG ICE Configurator utility MUST be run before starting a debug session. - When switching between different target boards be sure to first close the current debugger session, then move the emulator pod to the new target and finally start a new debugger session on the new target. "Hot swapping" between different target boards using "New Session" or "Select Session" from the debugger menu is not supported by the ICE. ====================================================================== Features in this release ====================================================================== - Added support for the ADSP-2126x family. ====================================================================== Fixes in this release ====================================================================== ====================================================================== Known Issues ====================================================================== - Limited support for ADSP-2126x external memory. Note that viewing external memory through a memory window may conflict with Parallel Port use by the target application. External memory accesses through the debugger is extrememly slow, this is being addressed. - Physically resetting the target processor is not supported while the ICE is connected and halted. If a reset must be applied then the target should be in a running state or the debugger should first be exited. - Memory fills using the "Memory->Fill..." command on either a 2106x or a 2116x will not be verified when "Verify all writes to target memory" is checked in the Target Options dialog. Loading programs and manually entering data into memory windows will be properly verified. - 21160 revision 0.x MS cycle counter register does not show proper value, it is a duplicate of the LS register. - Scrolling through MP memory regions on a 2106x device may cause the debugger to display invalid data in memory and register windows. To fix this, simply refresh the windows (F12 or Window->Refresh) and the correct data will be reloaded from the target. - Bits transfered to IMASKP from IRPTL upon servicing an interrupt, may be shifted right by 1 bit. This is a bug on ADSP-21160 Rev 0.0 and Rev 0.1 silicon. Rev 1.0 and higher parts fix this problem. ADSP-21161 All revisions up to 1.1 - On ADSP-2126x data hardware breakpoint 1 is not functional, please only use data hardware breakpoint 2. ====================================================================== Change Log ====================================================================== Revision 4.70.6 - Fixed TAR-15586 (External code memory load fails) - Fixed TAR-15584 (Fill of large PM ranges fails) - Fixed TAR-15424 (destructive read of DAI_IRPTL_H & DAI_IRPTL_L) - Fixed TAR-15379 (strange flags behavior) - Fixed TAR-15192 (flags register missing child bits) - Fixed TAR-15153 (using outdated register names) - Fixed TAR-15151 (external memory access) - Fixed TAR-14215 (data verification errors on 21160 & 21161) - Fixed TAR-14010 (failure to load large program correctly) - Fixed TAR-13887 (mode 2 shadow registers show non-existant bits) - Fixed TAR-13784 (tcl command dspload fails due to no 21262 support) - Fixed TAR-13761 (loading .dxe when using SPI boot mode) Revision 4.70.4 - Fixed TAR-15190 (wmsharcice.dl causes crash if configurator is not run first) - Fixed TAR-15154 (2116x, 2126x Emulator doesn't support DM_6464 memory type correctly) - Fixed TAR-14498 (2116x Extended register child bits are not getting set correctly) - Fixed TAR-14394 (2126x Emulator crashes VisualDSP when trying to load) - Fixed TAR-14330 (2126x Loading Any Program Crashes Emulator) - Fixed TAR-14237 (21161 code in ext 32 mem packed incorrectly) - Fixed TAR-14039 (Readme file for Sharc HPPCI-ICE indicates only VisualDSP++ 3.0) - Fixed TAR-13926 (Update readme HPPCI-ICE & Summit-ICE) Revision 4.60.6 - Fixed issue with online help not working with Target Options Revision 4.60.5 - Fixed some issues so that we can work with the new configurator - Fixed issue of multiple emulator instances (TAR-3013) - Fixed CB7S & CB15S registers in STKYX (TAR-12355) Revision 4.60.4 - There were still some issues with double writes that are now fixed Revision 4.60.3 - Fixed issue with double memory writes on 21160N Rev 0.1. Revision 4.60.2 - Fixed issue with writing to some children bits in IOP registers on 2116x. - Removed duplicate bits and non-existent registers from the 21065L custom register window. This included duplicate SYSTAT, WAIT, STCTLx, and SRCTLx bits and the removal of DMAC6, DMAC7, and KEYMASKx registers. - Added RBWM and RBWS bits to the WAIT register on 21161. - Removed cache registers from 2116x sessions since the contents are invalid while using the ICE. The cache register menu items are now disabled while using an ICE session. Revision 4.60.1 - Ability to acknowledge a core hang without having to reset or exit. This allows the user to switch focus and potentially clear the hang condition. - Added detection for SPI boot mode on the ADSP-21161. After a reset the PC will now be located at 0x40005. - Added SPI control register definitions for the ADSP-21161. - Added SPORT control register definitions for the ADSP-21161. Revision 4.50.0 - Support for the 21160 revision 1.x. - Fixed problems seen in multi-processor sessions when changing focus if a shared external memory window was open. - Fixed a problem on 21161 involving bits shifting in the IMASKP register. The IMASKP register is now read-only from within the debugger. Revision 4.40.0 - Added support for writing to 48-bit memory on revision 1.x 21160 parts which would cause duplicate writes to occur. - More robust multi-processor sessions. Revision 4.30.0 - Added support for ADSP-21161 processor. Revision 4.20.1 - Fixed Core Hang bugs during startup and loading.