====================================================================== - Wm219xIceHP - ADSP-219x HPPCI-ICE JTAG Emulator Debug Target DLL Version 1.00.2 Analog Devices, Inc. ====================================================================== Wm219xIceHP is a ADSP-219x JTAG Debug Target for VisualDSP++ 2.0 or greater. It will provide full JTAG debug support for ADSP-219x processors using the HPPCI-ICE from Analog Devices. ====================================================================== Requirements ====================================================================== - VisualDSP++ 2.0 or greater with 219x support - HPPCI-ICE JTAG emulator from Analog Devices - Windows 95 OSR2, Windows 98, Windows NT 4.0 with SP3 or greater, Windows 2000, or Windows XP ====================================================================== Installation and Usage Notes ====================================================================== - Operation under Windows NT, Windows 2000 or Windows XP requires the proper JTAG Emulator Driver from Analog Devices, Inc. to be installed and running. The driver installation is integrated into the Emulation Tools setup for Windows NT. - After installation the JTAG ICE Configurator utility MUST be run before starting a debug session. - When switching between different target boards be sure to first close the current debugger session, then move the emulator pod to the new target and finally start a new debugger session on the new target. "Hot swapping" between different target boards using "New Session" or "Select Session" from the debugger menu is not supported by the ICE. ====================================================================== Features in this release ====================================================================== - Initial release - Run, halt, step, reset, and restart for both single and synchronous multi-processor targets - Read, write, fill memory and load executables - Read and write registers - High performance stistical profiling - High performance Background Telemetry Channel (BTC) ====================================================================== Fixes in this release ====================================================================== - Extended Registers were not showing up under the Register Menu ====================================================================== Known Issues ====================================================================== - For the 2191, the trace buffers are enabled/disabled using the 13th bit in the ICNTL register(1-enable, 0-disable). If a user's program clears the 13th bit in ICNTL then NO trace buffer information will be collected. ====================================================================== Change Log ====================================================================== Revision 1.00.1 - TAR-14552 (Frequency selection dialog crashes debugger) - TAR-15641 (Summit/HPPCI ICE enable statistical profile 2195/2196)