AD8370 Evaluation Board Control Software Rev.2 


To control the AD8370 evaluation board, you simply have to copy the AD8370_Rev2_DGA_SW.exe file to any location on your computer and run it.

You must have the Microsoft Visual Basic 6.0 runtime engine installed on your PC before you can run the program.  If you do not have it installed you may have to run the setup file, vbrun60sp5.exe. 



Additional Notes for users operating Windows 95/NT/2000:

The AD8370 Control Software requires direct hardware I/o access to the parallel port of the PC.

If you are running Windows 95/NT/2000 and receive the error message 

	"Run-time error 53: File not found: dlportio.dll"

it will be necessary to install the Windows 95/NT Port I/O driver, port95nt.exe.

This port95nt.exe file is provided in the AD8370 software package and is only needed if you get this error.

A system reboot may be required after installation of the port driver.