WirelessHART adopted as a China GB/T national standard

2014年05月23日

Figure 1

   

The HART Communication Protocol (including WirelessHART) has been approved as China National Standard, GB/T 29910.1 ~ 6-2013. This was officially announced at a special press briefing in Beijing, hosted by the HART Communications Foundation and sponsored by Emerson Process and Linear Technology.

 Already an international standard (IEC62591), WirelessHART’s adoption as a China national standard will further drive adoption of WirelessHART in China, and is just the latest sign of widespread acceptance of WirelessHART systems. 

Learn more about WirelessHART solutions.

WirelessHART China Std - press event

May 8, 2014 (Beijing) - HART Communication Foundation press event, announcing the standard GB/T 29910.1~6-2013

著者について

Ross Yu
Ross Yu is the Product Marketing Manager at Linear Technology for the Dust Networks product line. Mr. Yu and his team at Dust Networks have made significant contributions to solving the challenges inherent in the exciting
myAnalogに追加

myAnalog のリソース セクション、既存のプロジェクト、または新しいプロジェクトに記事を追加します。

新規プロジェクトを作成

この記事に関して