Adjustable Low-Battery Threshold Detector Extends Battery Runtime

2001年09月01日

Figure 1

   

The LTC1998 is the first Lithium-Ion low-battery detector that guarantees 1% accuracy even when using inexpensive 1% programming resistors. This device facilitates more reliable battery capacity management; it extends battery runtime and improves prediction of remaining battery charge. The LTC1998 achieves this performance by combining an accurate internal reference and a proprietary comparison circuit. Other features include:

  • Low supply current, 2.5µA typical
  • Adjustable low-battery threshold, 2.5V to 3.25V
  • Adjustable hysteresis, 10mV to 750mV
  • Rail-to-rail push-pull output eliminates pullup resistor
  • Dedicated output supply pin ensures compatibility with microprocessors
  • Small ThinSOT 6-lead SOT-23 Package

The LTC1998, in the SOT-23 package, compares the voltage of a single Lithium-Ion cell to an internal reference voltage. When the battery voltage falls below a predetermined low-battery threshold, the output pin (BATTLO) changes state to indicate a low-battery condition. The low-battery threshold voltage is adjustable from 2.5V to 3.25V via the threshold adjust pin. The threshold voltage is guaranteed to be within 1% of the programmed voltage as long as the threshold-adjust pin voltage is programmed with a resistor divider composed of 1% or better resistors. The BATTLO output of the LTC1998 can be used by a microprocessor or microcontroller in a battery-powered system to ensure that the battery has sufficient remaining capacity to allow proper operation or ensure that stored settings are not lost. The high accuracy of the LTC1998 improves the ability of the system to predict the remaining battery capacity. The LTC1998 can provide a longer runtime than a system using a less accurate threshold detector since it requires a smaller guardband for detector error. The LTC1998 can also be used to protect a battery from damage from overdischarge. In addition, the 2.5µA typical supply current is less than the effective self-discharge current of most Li-Ion cells.

In many applications, the system reduces the battery load current during a low-battery condition, thus allowing the battery voltage to recover over time. The large adjustable hysteresis of the LTC1998 allows it to ignore this voltage change so that the output does not change state to indicate a false recharged battery condition. The hysteresis is programmable via the hysteresis-adjust pin.

Programmable Thresholds

An accurate internal reference and internal divider set the low-battery threshold level at which the BATTLO signal changes from high to low. The threshold can be adjusted via the threshold-adjust pin (VTH.A), as in Figure 1. A proprietary threshold adjustment circuit maintains a highly accurate threshold voltage even when using 1% external resistors to set the threshold voltage. This gives the LTC1998 the accuracy of a trimmed fixed-threshold device as well as the flexibility of an adjustable threshold.

Figure 1. Threshold adjustment with resistor divider.

Hysteresis is programmable via the hysteresis-adjust pin VH.A). This pin works in exactly the same way as the low-battery threshold adjust pin, except that it controls the threshold at which the BATTLO signal changes state from low to high, indicating a charged battery condition. Both the low-battery threshold voltage and the hysteresis-threshold voltage may be programmed to be between 2.5V and 3.25V; the hysteresis is the difference between these two thresholds. The hysteresis may be as large as 750mV. This large hysteresis prevents false state changes at the output due to transients or battery recovery. The system may then be designed to automatically reduce the battery load current when a battery-low signal is received. If the battery voltage recovers under this reduced load, the output of the LTC1998 will maintain a low output state. Both thresholds may be programmed using just three external resistors, as shown in Figure 2, minimizing component count. The threshold-adjust and hysteresis-adjust pins exhibit very high input impedance, which allows the use of large external program resistors to reduce the battery drain current.

Figure 2. Single resistor divider sets both thresholds.

The threshold-adjust function is continuous; threshold voltages can be adjusted at any time and changes take effect instantaneously, without the use of a clock or reset. This allows simple switched resistors to change thresholds. Figure 3 illustrates how a system can be designed with multiple low-battery threshold levels. In such an application, the load current can be reduced when a low-battery signal is produced. For example, the application can change the low-battery threshold to a lower voltage with S1 and continue to run in a low power mode, keeping system parameters stored safely in memory. When the battery voltage finally drops below the new low-battery threshold, the system can be shut down completely in order to protect the battery from damage due to overdischarging.

Figure 3. Dual low-battery threshold circuit.

Versatile Output Stage

The LTC1998’s BATTLO output is a rail-to-rail push-pull CMOS output driver with a dedicated driver supply pin, VLOGIC. A break-before-make circuit prevents power supply cross-conduction currents during switching to reduce battery load transients. The VLOGIC pin may be wired to BATT or driven by a lower supply voltage to allow compatibility with low voltage microprocessors (Figure 4). The BATTLO pin will drive a high output signal to the voltage set by the VLOGIC pin. The VLOGIC pin can be any voltage between 1V and VBATT. This feature helps to protect a low voltage microprocessor or microcontroller from overvoltage stress at its battery-threshold detect input pin. The VLOGIC pin can also be driven from a separate supply so that output drive current is not taken from the battery, further increasing battery life. The BATTLO output can drive a voltage that is a higher potential than the BATT pin, provided that a resistor is connected from the VLOGIC pin to the required supply, as in Figure 5.

Figure 4. VLOGIC pin ensures compatibility with processor logic level.

Figure 5. Simple pull-up resistor increases compatible logic range.

Conclusion

The LTC1998 low-battery threshold detector provides a small (SOT-23-6), accurate, low power solution to capacity management problems in Lithium-Ion battery applications. It can improve useful battery life and is flexible enough to work in many different applications. Low cost 1% resistors can be used to configure thresholds while maintaining 1% threshold accuracy. Its ultralow power consumption minimizes battery drain current.

著者について

Brendan Whelan
Brendan Whelanは、アナログ・デバイセズでスイッチ/マルチプレクサ/リファレンス/温度センサー製品を担当する設計ディレクタです。電圧リファレンスやシリコン・ベースの温度センサーなどの高精度DC製品、シリコン・スイッチ、MEMSスイッチの設計を統括しています。ゼロドリフト・アンプ、電流検出IC、様々なオーディオ回路などの設計に携わってきました。いくつかの特許を保有するほか、技術記事の執筆や動画の制作にも従事。レンセラー工科大学で電...
myAnalogに追加

myAnalog のリソース セクション、既存のプロジェクト、または新しいプロジェクトに記事を追加します。

新規プロジェクトを作成

この記事に関して

最新メディア 21
Title
Subtitle
さらに詳しく
myAnalogに追加

myAnalog のリソース セクション、既存のプロジェクト、または新しいプロジェクトに記事を追加します。

新規プロジェクトを作成