Thermocouple TechClip
2017年09月18日
LTC2983は高精度で使いやすい万能温度測定システムです。熱電対と直接インタフェースすることができ、熱電対の出力電圧と冷接点温度を同時に測定し、結果を摂氏と華氏で報告します。外部リファレンス、バッファ、レベル・シフト回路は不要です。標準的熱電対用の直線化データを備えています。あるい表データを使ってカスタム熱電対用にプログラムすることができます。それぞれの結果にはセンサ固有のフォルト・データが含まれます。
LTC2983は20個のアナログ入力を備えており、それらは広くE、J、K、N、T、B、S、およびRタイプの熱電対、ダイオード、サーミスタ、およびRTDをデジタル化するように設定することができます。サーミスタやRTDに対するLTC2983のユニークな機能についてはこのシリーズの他のビデオを参照してください。
Thermocouple TechClip
2017年09月18日
LTC2983は高精度で使いやすい万能温度測定システムです。熱電対と直接インタフェースすることができ、熱電対の出力電圧と冷接点温度を同時に測定し、結果を摂氏と華氏で報告します。外部リファレンス、バッファ、レベル・シフト回路は不要です。標準的熱電対用の直線化データを備えています。あるい表データを使ってカスタム熱電対用にプログラムすることができます。それぞれの結果にはセンサ固有のフォルト・データが含まれます。
LTC2983は20個のアナログ入力を備えており、それらは広くE、J、K、N、T、B、S、およびRタイプの熱電対、ダイオード、サーミスタ、およびRTDをデジタル化するように設定することができます。サーミスタやRTDに対するLTC2983のユニークな機能についてはこのシリーズの他のビデオを参照してください。
LTC2983 製品詳細ページ
LTC2983は20個のアナログ入力を備えており、それらは広くE、J、K、N、T、B、S、およびRタイプの熱電対、ダイオード、サーミスタ、およびRTDをデジタル化するように設定することができます。サーミスタやRTDに対するLTC2983のユニークな機能についてはこのシリーズの他のビデオを参照してください。
{{modalTitle}}
{{modalDescription}}
{{dropdownTitle}}
- {{defaultSelectedText}} {{#each projectNames}}
- {{name}} {{/each}} {{#if newProjectText}}
-
{{newProjectText}}
{{/if}}
{{newProjectTitle}}
{{projectNameErrorText}}