faqs
よくある質問(FAQ)
Can I use the ADV202/212 if my input is not to standard NTSC, PAL, 720p/60, 1080i/60 video?
Yes. If the input is to vary only in vertical and horizontal active and/or total resolution and is accompanied by HVF or EAV/SAV codes, Custom Specific mode can be used. In this mode the user defines active resolution and total resolution in writing to specific dimension registers.
Refer to the Programming Guide for details on Custom Specific Mode.