RF Converters Enable Multiple Wideband Applications

This webcast will focus on the advantages and flexibility that RF data converters bring to a radio designer, especially with the higher data rates that recent advances in converter technology have enabled. Radio applications such as wireless infrastructure, cable headend transmitters, radar, and instrumentation can all be implemented and simplified through the use of RF converters. Examples of transmitters using RF DACs will be shown.


Daniel E. Fagueは、アナログ・デバイセズの高速プロダクトグループのシステム・アプリケーション・エンジニアリング・ディレクターです。1989年にゴンザガ大学で電気工学の学士号、1991年にカリフォルニア大学デービス校で電気工学の修士号を取得しています。1995年に入社し、ワイヤレス・ハンドセット・グループにおいて、GSM、EDGE、CDMA、Bluetooth用のダイレクト・コンバージョン無線を含む無線ハンドセットのアーキテクチャ設計を担当しました。入社する前は、National Semiconductor社でDECTやPHS向けの無線アーキテクチャの設計に5年間携わっていました。2011年に高速プロダクトグループに属してからは、主にRF コンバータの開発に取り組んでいます。7件の特許を保有し、これまでに30本以上の記事や論文を発表しています。