Demystifying the JESD204B High-Speed Data Converter-to-FPGA Interface

This webcast will provide an overview of the JESD204 standard from its original version up to the current "B" revision. In addition, common "high-performance metrics" that are associated with high speed serial interfaces such as JESD204 will be described. Topics covered in this webcast will also be useful for applications that use similar high speed serial interfaces.

 

 

  • Presenter
  • Jonathan Harris

    Product Applications Engineer

Jonathan Harrisは、アナログ・デバイセズのプロダクト・アプリケーション・エンジニアです。米ノースカロライナ州グリーンズボロにある航空製品部門に所属しています。RF製品を担当するアプリケーション・エンジニアとして10年以上の業務経験を持ちます。ノースカロライナ大学シャーロット校で学士号、オーバーン大学で修士号を取得しています。休日には家族との時間を大事にするとともに、オートバイやフットボール、モバイル・オーディオなども楽しんでいます。