製品概要

製品概要

The ADF7020 evaluation board software controls the operation of the ADF7020 evaluation boards from a PC over a USB . Install the ADF7020 evaluation software by clicking on "ADF7xxx_ADIismLINK Install_*.exe" at the link provided. The software will be available under Programs → Analog Devices → ADF7xxx . The Analog Devices example network protocol software, ADIismLINK Rev2.0, is also installed as part of this setup file: Programs → Analog Devices → ADIismLINK V2 Host Application.

ADF7020 schematic and BOM are included in the Evaluation Board User Guide.

はじめに

ADF7020 Evaluation Board User Guide is installed with the software.

推奨システム動作環境

  • Eval-ADF70XXMBZ2 mother board required to work with the Eval-ADF7020DBx daughter board.
  • Evaluation software is compatible with Windows XP/Windows Vista/Windows 7.

ソフトウェア

Code Examples

ZIP
6 kB
ADF7xxx Device Driver Codes - Blackfin
Provides the c code source files allowing configuration using the ADSP-BF53X, Blackfin DSP processor. Routines to write the configuration values are provided as well as routines allowing a simple RF link to be setup between two ADF7020 devices. Please refer to application note AN-771 for details on the hardware connections.
ZIP
15 kB
ADF7xxx Device Driver Codes - Microconverter
Provides the c code source files allowing configuration using an 8052 based microcontroller. Routines in this file will have to be adapted depending on the MCU and compiler used. This version uses the ADuC845/ADUC847 Microconverter from Analog Devices. The code was developed using the Keil C51 compiler within their uVision IDE.

評価用ソフトウェア

ZIP
25403 kB
ADF70xx Evaluation Software
The most up-to-date ADF70xx software download is bundled with all documentation, including schematics, for the ADF70xx family of transceivers. Layout can be found in the gerber files under the documentation tab.

設計ツール

ADIsimSRD デザインスタジオ
アナログ・デバイセズのADIsimSRD Design Studioはきわめて強力なツールであり、ADF7xxxファミリーである トランシーバとトランスミッタ製品を使用して、標準的なワイヤレス・システムの多くのパラメータをリアルタイムにシミュレートして最適化します。

購入

PCサイトでは製品の購入が可能です。
価格は1個当たりの米ドルで、米国内における販売価格(FOB)で表示されておりますので、予算のためにのみご使用いただけます。 また、その価格は変更されることがあります。米国以外のお客様への価格は、輸送費、各国の税金、手数料、為替レートにより決定されます。価格・納期等の詳細情報については、弊社正規販売代理店または担当営業にお問い合わせください。なお、 評価用ボードおよび評価用キットの表示価格は1個構成としての価格です。