TD-SCDMA RD V2.1 Design Meets Rx-Blocking Mask and Sensitivity Requirements

Abstract

This application note introduces Maxim's 2nd-generation TD-SCDMA radio frequency transceiver chipset with its V2.1 reference design. It also discusses some of the key system issues, such as sensitivity and blocker tests, that warrant careful consideration in order to create an optimum TD-SCDMA RF design.

Maxim TD-SCDMA RF Transceiver Chipset

Maxim's TD-SCDMA mobile-phone RF chipset consists of the MAX2507 (Tx) and the MAX2392 (Rx). Both RF ICs are fabricated using Maxim's in-house, high-frequency process technology. The MAX2507 is a fully-integrated transmitter chip that includes circuits from analog I/Q input to power-amplifier output. Its main functional blocks include an I/Q quadrature modulator, an upconverter, a variable-gain amplifier (VGA), an RF voltage-controlled oscillator (VCO) and phase-locked loop (PLL), IF local oscillator generation, and an RF power amplifier (PA). This device is packaged in a 7mm x 7mm land grid array (LGA). The companion zero-IF receiver, the MAX2392, includes circuits from a low-noise amplifier (LNA) to analog I/Q output. Its main functional blocks include an LNA, an RF I/Q demodulator, RF VCO and PLL circuitry, baseband channel-select filters, DC-offset correction circuitry, and automatic gain control (AGC) baseband amplifiers. The MAX2392 is housed in a 5mm x 5mm QFN package. A complete reference design that facilitates the OEM radio RF board design shows an effective overall PCB size of 6.6cm². The functional block diagram of the reference design is shown in Figure 1 and a photograph of the reference board in Figure 2.

Rx Requirements in TD-SCDMA Standard

The main Rx requirements of the TD-SCDMA standard are shown in Table 1. The minimum sensitivity that needs to be met is -108dBm, while the blocking spec is a canyon shape with frequency offset.

Figure 1. TD-SCDMA reference-design functional block diagram.
Figure 1. TD-SCDMA reference-design functional block diagram.

Figure 2. TD-SCDMA reference design board.
Figure 2. TD-SCDMA reference design board.

Table 1. TD-SCDMA Rx Requirements

General Requirements
Description Spec Note
Frequency Band 2010MHz to 2025MHz
BER < 0.001
Eb/Nt 5.2dB
  • Estimation/simulation
  • Subject to change
  • Rx Sensitivity -108dBm 12.2kbps data rate
    Maximum Input Level -25dBm/1.28MHz DPCH_Ec/Ior is 7dB
    Adjacent Channel Selectivity (ACS) 33dB ±1.6MHz frequency offset
    Receiver System NF < 6.8dB Customer proposed
    I and Q Output Power 1VP-P with 2kΩ loading Customer proposed
    I and Q LPF Requirements -40dBc at 5.12MHz,
    -3dBc at 800kHz,
    Bessel response with 3°
    phase delay and 0.2dB amp
    ripple below 640kHz
  • Customer proposed
  • Design with MAX4134 op amp

  • Blocking Requirements
    In-Band Blocking Case 1 Case 2
    Blocking Offset ±3.2MHz ±4.8MHz
    Desired Signal Level -105dBm/1.28MHz -105dBm/1.28MHz
    Undesired Signal Level (Modulated) -61dBm/1.28MHz -49dBm/1.28MHz

    Out-of-Band Blocking
    Parameter Band 1 Band 2 Band 3 Unit
    Desired Signal Level -105 -105 -105 dBm/1.28MHz
    Undesired Signal Level (CW) -44 -30 -15 dBm
    Frequency Band 1840 < f < 1885
    1935 < f < 1995
    2040 < f < 2095
    1815 < f < 1840
    2095 < f < 2120
    1 < f < 1815
    2120 < f < 12750
    MHz

    Sensitivity and Blocking Spec Analysis and Measured Results

    Receiver sensitivity is a system specification that is very much influenced by the signal quality in the RF channel and the baseband processing in the DSP modem section. Under minimum input signal level conditions, the RF channel quality is purely limited by the receiver's noise contribution, which is determined by its noise figure (NF). Note that, under these signal conditions, receiver phase noise is not considered because its level is much smaller than that of thermal noise. Therefore, receiver phase noise has minimal impact on the degradation of the input SNR. In the 3GPP TR 25.945 standard [3], receiver sensitivity is specified at -108dBm. Based on typical baseband processing gain and desired BER after demodulation, this receiver sensitivity corresponds to a 9dB maximum receiver NF. The measured NF of the TD-SCDMA reference design receiver path, shown in Figure 1, is around 5.7dB. Hence, the corresponding measured sensitivity is -111dBm, which allows for 3dB additional margin over the standard specification.

    The effects of in-band blockers on receiver performance are typically manifested in three phenomena: cross-modulation, 2nd-order intermodulation products, and reciprocal mixing, which are discussed in the following three subsections.

    Cross-Modulation

    Figure 3. Cross-modulation products.
    Figure 3. Cross-modulation products.

    Figure 3 shows the cross-modulation phenomenon that occurs in a nonlinear component such as an amplifier or a mixer. In the figure, the signal at f1 is a modulated blocker with a certain bandwidth, and the CW signal at f2 represents the desired signal. At the amplifier output, a triangular intermodulation product results at f2 centered around the desired signal-frequency spectrum. This cross-modulation product is typically related to the component's 3rd-order nonlinearity characteristics and, hence, its 3rd-order intercept point. When the blocking signal has a Gaussian-noise-like normal distribution, the power of the resulting cross-modulation product can be estimated using the following formula:

    Equation 1

    In the case when the input signal is also modulated, the shape of the output product is the convolution of a triangle and the signal-power spectral-density function. As the blocker characteristics deviate from the Gaussian noise-like normal distribution, the cross-modulation product becomes smaller. When the interfering signal is considered as a modulated blocker with a constant envelope, the cross-modulation product is zero.

    The 3GPP TDD standard specifies that 3dB degradation in sensitivity is allowed for a -49dBm modulated interferer at a ±4.8MHz offset. If we consider that the sensitivity degradation results solely from the cross-modulation product, this performance level is achievable as long as the power of the cross-modulation product is small in relation to the power of the receiver's in-band thermal noise at sensitivity level. Assuming that noise figure of the receiver is less than 9dB, as required by the standard, we can deduce from equation 2 the equivalent receiver's 3rd-order intercept point, as dictated by cross-modulation.

    Equation 1

    2nd-Order Intermodulation Products (IM2)

    Figure 4. 2nd-order intermodulation products.
    Figure 4. 2nd-order intermodulation products.

    The 2nd-order intermodulation products due to a modulated blocker consist of three components, as shown in Figure 4: DC offset, low-frequency products around 0Hz, and products around 2f1. When the blocker's signal statistics follow a Gaussian-noise-like normal distribution, the three components are equal in power, and they can be estimated using the formulas shown in Figure 4. When the blocker's signal statistics approach those of a constant envelope signal, the power level of the low-frequency products gets minimized. When the interfering signal is a constant envelope blocker, there are no low-frequency IM2 products generated at the output. At the I/Q outputs of a zero-IF receiver, these low-frequency and DC IM2 components fall in the desired downconverted signal band and can result in receiver performance degradation. In the MAX2392 receiver circuitry, DC offsets are removed on-chip; therefore, only the low-frequency IM2 products need to be accounted for when looking at the receiver interference budget.

    The 3GPP TDD standard specifies that 3dB degradation in sensitivity is allowed for a -49dBm modulated interferer at a ±4.8MHz offset. Similar to the cross-modulation case, if we consider that the sensitivity degradation results solely from low-frequency IM2 products, and the NF of the receiver is less than 9dB as required by the standard, we can estimate the required receiver 2nd-order intercept point, IIP2,RX, as shown in equation 3. Assuming that the downconverted in-band blockers are eliminated in the post-mixer baseband channel-select filters, the receiver 2nd-order intercept point is solely dictated by that of the zero-IF downconverter block.

    Equation 3

    Note: The term "-3" is dependant upon the modulation index.

    There are four operational modes of the MAX2392. The high-gain high-linearity (HGHL) and high-gain medium-linearity (HGML) modes are recommended for receiving a weak signal in the presence of a large blocker. Both modes result in measured IIP2,RX > +15dBm for the reference-design receiver section, which meets the requirement by at least 12dB of margin.

    Phase Noise and Reciprocal Mixing

    The 3GPP TD-SCDMA standard does not explicitly specify the phase noise of the VCO; instead it is derived from other specifications that depend on it. Transmitter EVM is one of the parameters that is impacted by the transmitter's VCO+PLL phase noise, as previously described, though it does not place a stringent phase-noise requirement on the radio. Receiver sensitivity is also dependent on LO phase noise, but it also does not place a stringent phase-noise requirement on the radio, even in the case of 16QAM modulation. Two specifications that tend to impose stringent specifications on LO phase noise are the blocking and two-tone intermodulation characteristics minimum requirements. These imposed specifications are manifested in a phenomenon referred to as reciprocal mixing, or the modulation of the LO sideband noise onto an interferer, as demonstrated in Figure 5.

    Figure 5. Reciprocal mixing of LO phase noise onto an inteferer.
    Figure 5. Reciprocal mixing of LO phase noise onto an interferer.

    As mentioned in the discussion of blocking and two-tone intermodulation requirements, receiver sensitivity is allowed to degrade by 3dB in these test scenarios. We assume that all degradation is due to the phase-noise reciprocal mixing, and the receiver noise figure is less than 9dB as required by the standard. We can then deduce the required LO phase noise using the following equation:

    Equation 4

    The maximum interference power noted in the blocking and two-tone intermodulation test cases is a -46dBm tone at ±3.2MHz offset from the desired signal center frequency. Substituting this value into the above equation, we get a requirement for receiver LO phase noise to be less than -119dBc/Hz at 3.2MHz offset from the carrier. The measured phase noise of the MAX2392 VCO is -129dBc/Hz, which meets the requirement with 10dB of margin.

    For out-of-band blocking, the SAW filter before the LNA knocks down all out-of-band interferences to an acceptable level to avoid LNA compression. The SAW filter between the LNA and mixer may not be needed because the blocker level at the LNA output is already low enough as compared with the mixer IP2 and IP3. An interstage filter provides the required balun function, so the additional filtering benefit is provided at no extra cost. For example, at ±85MHz offset, the specified blocker is -15dBm. If the SAW provides 30dB attenuation, the blocker level at LNA is -46dBm (1dB loss from T/R switch), which is similar to the in-band blocker level and can be analyzed by the above method in terms of IM2 and IM3. Measured results suggest that there is at least 3dB of margin from 3GPP requirements in each blocker test.

    Summary

    Maxim's TD-SCDMA reference design V2.1 fully meets the 3GPP standard requirements with at least 3dB of margin for all key receiver specifications.