Industrial Ethernet
Scalable Ethernet, Timed to Perfection
ADI Chronous™ is the leading portfolio of edge-to-enterprise Industrial Ethernet connectivity solutions, specifically designed to accelerate your path to Industry 4.0. ADI has leveraged its deep domain expertise and advanced technologies to help partners connect the industrial devices and networks of the future. Our trusted solutions ensure your critical data is reliably delivered throughout your application, ensuring seamless connectivity and operational efficiency. ADI Chronous solutions stand up in the toughest, time-critical environments and opens the door to time-sensitive networking.
The Path to Industry 4.0
Communications infrastructure is the backbone of the connected factory and presents many key opportunities on the path to Industry 4.0. As networks pivot from legacy fieldbus to Industrial Ethernet, multiple challenges emerge within the design and implementation phases. Developing future-proofed, robust, and scalable Industrial Ethernet solutions that can support multiple protocols is a time consuming and resource intensive task. It necessitates a pivot in skillsets and knowledge base to architect systems that ensure data integration, synchronization, and system interoperability. There is, however, a trusted partner who can help you navigate this task, assist in the design and development of seamless, robust Ethernet solutions: Analog Devices.

Deterministic Ethernet for Industry 4.0 Applications
See how this technology provides determinism at the node for factory devices so they do not have to worry about the effects of network traffic.

An Introduction on Implementing Industrial Ethernet
One obstacle that sometimes gets in the way of updating industrial protocols to Ethernet is an unclear implementation plan. This article looks at how an industrial plant might get started on the road from field bus to Ethernet.
Benefits of ADI Chronous™ Products
The suite of Industrial Ethernet products includes technologies, solutions, software, and security capabilities designed to connect the real world to factory networks and beyond to the cloud. ADI leverages 50 years of experience supplying factories with industrial connectivity and next-generation Industrial Ethernet technologies that solve the big challenges surrounding seamless and secure edge-to-cloud connectivity.
Industrial Ethernet products include switches, physical transceivers, controllers, and network interface modules with full software protocol stacks. Designed to support scalable and flexible system development, the ADI Chronous™ portfolio offers multiple port count, low power consumption, and flexible bandwidth. Being multiprotocol, these solutions are compatible with all existing protocols while also providing the ability to future-proof for TSN features. Get to market fast with predicable, trusted results you can depend on every time by building your design with ADI’s robust Industrial Ethernet solutions.

![]() |
Deterministic
For Precision Control
![]() |
Verified Robust
For the Harshest Conditions
![]() |
Scalable
For Optimized System Design
Delivering Trusted Data in Key Application Areas
ADI Chronous solutions are designed and verified for robust operation in harsh industrial environments and offer effective security at each node point within a system. ADI’s understanding of network architectures coupled with its application knowledge of how data is collected, processed, and used throughout an operation all serve to inform the security and robust features present in the ADI Chronous offerings. These features make ADI Chronous an ideal choice for a number of markets.
Process and Factory Automation
Deterministic networks and gigabit performance is a requirement of the future factory or process automation system. ADI Chronous, delivers off-the-shelf, full featured solutions that reduce development effort, risk, and time to market for new standard adoption.
Connection Motion and Robotics
ADI’s Chronous enables synchronization across the boundary of the network into the application, from sub-1 μs right down to the PWM outputs within the servo motor control. This improves machining and production accuracy in multi-axis applications such as robotics and CNC machines.
Building Automation
Addressing the multiple bandwidth requirements of existing and future intelligent buildings, ADI Chronous provides reliable, secure, and trusted digital communications at all levels of the network.

Time Sensitive Networking (TSN) with ADI Chronous
ADI Chronous solutions are designed to address the requirements of time sensitive networking (TSN) and deterministic Ethernet. Time sensitive networking, or TSN, refers to a group of IEEE 802.1™ and IEEE 802.3™ standards developed to provide deterministic performance within standard Ethernet. It is a universal standard being developed at an industry level to eliminate interoperability problems between protocols. It allows current protocols to share networks and provide reliable deterministic communication and scalability across applications, bandwidths, and enterprises all the way to the edge node. Given that the TSN standard is nearly finalized, now is the time to practically deploy standard Ethernet (with the TSN extensions) in real-time, mission critical applications. New hardware and software will be required that can support all these TSN features and ADI Chronous is the ideal solution for scalable, robust solutions that are designed for ease of deployment.
The ADI Chronous portfolio is supported by a host of software elements that simplify the adoption and increase the reliability of each product offering. Supporting multiple protocols, ADI offers a choice of fully tested and verified, production ready software protocol stacks that accompany our hardware. From host software drivers to APIs and development tools, ADI has the software needed to make the adoption of new standards and technology quick and simple.
Integrated with ADI’s PriorityChannel™ Technology
The Developer Portal provides additional information, resources and support for registered users who are evaluating the ADI Chronous embedded switches and network interface modules. Register to explore the content and simplify your Industrial Ethernet designs.
Developer Portal gives access to:
- The latest hardware reference design schematics
- A suite of network software for all protocols
- Documentation and development tools
Already have an account? Log in now



TECHNOLOGIES
ARE MAKING A
GLOBAL IMPACT
TECHNOLOGIES
ARE MAKING A
GLOBAL IMPACT
Latest Resources
Videos
- New ADIN1100: Ultra Low Power, Robust, 10Base-T1L PHY
- The Future of Ethernet Connectivity in Industrial Systems
- ADI: The Future of Ethernet Physical Layers in Industry 4.0
- Pervasive Sensing: The Thread Running Through Industry 4.0
- From Now to Next: Accelerating the Path to Industry 4.0
Article
Press Release
Product Information
Protocol Certifications
Technical Articles Page
- Enabling Seamless Ethernet to the Field with 10BASE-T1L Connectivity
- Time Sensitive Networking: Five Ways the IEEE Standards Will Advance Industry 4.0
- Ethernet-APL: Optimization of Process Automation with Actionable Insights
- Robust Ethernet Physical Layer Solutions for Time Critical Communications in Harsh Industrial Environments
- Accelerating the Transition to Industry 4.0 with Industrial Ethernet Connectivity