Industrial Ethernet Physical Layer Devices
Our industry-leading low latency and low power PHY technology maximizes data transmission and signal integrity in deterministic applications by reducing cycle times and system power consumption. It enables superior synchronization of signals across the industrial network and supports the development of TSN.
This portfolio of ultra low power 10BASE-T1L products includes both PHY and MAC PHY solutions to support optimization of system power budgets while offering flexibility in design choice. The unique MAC PHY technology enables the reuse of existing low power processor technologies that do not support traditional Ethernet interfaces, and instead enable connection via SPI.
Having completed extensive EMC and robustness testing, ADI Chronous PHY products are ideally suited for applications demanding predictable and secure communications. Designed to operate over an extended industrial ambient temperature ranges, Industrial Ethernet physical layer devices provide the highest level of reliability for the Industrial Ethernet applications of today and tomorrow.
What Is 10-BASE-T1L?
The IEEE 802.3cg™-2019 standard governs 10BASE-T1L connectivity. It is a single-pair Ethernet (SPE) media standard, providing for 10 megabits per second communication and enabling both power and data over single twisted pair cabling up to 1 km.
10BASE-T1L physical layer transceivers, part of the ADI Chronous™ portfolio, will enable Ethernet connectivity to edge nodes and direct IP addressability. Our technology enables the communication of new insights about process variables or building parameters to control systems. This will enable the optimization of asset utilization in process control and drive building management efficiencies.
Application-Level Value
Lower Cost Single Twisted Pair Cabling
Lighter, lower cost, and smaller size than standard CATx cables, these cables are also often easier to install. 10BASE-T1L technology will enable the reuse of some existing single twisted pair cabling infrastructure.
Long 1 km Reach
Field sensors are often deployed in remote locations, and existing Ethernet physical layer technologies are typically limited to 100 meters. The longer transmission distance enables longer distance device connectivity.
New Insights with 10 Mbps
This significant bandwidth increase over technologies like 4 mA to 20 mA or field bus provides the ability to transfer new insights from remote nodes.
Power and Data on Two Wires
Field sensors require power, and the ability to deliver power over the cable is critical for remote locations. The standard helps deliver up to 500 mW of power within intrinsically safe applications and 60 W within non-intrinsically safe applications. This is cable dependent.
Intrinsically Safe Application
Extends Ethernet to hazardous locations by supporting deployment in intrinsically safe applications, Zone 0/Zone 1 regions.
New Data, New Insights with 10BASE-T1L
Long reach, single-pair Ethernet, 10BASE-T1L physical layer devices are proving a game changer on the road to realizing the Industry 4.0 vision of seamless connectivity. By extending Ethernet connectivity to edge nodes in remote and distant locations, this technology enables new data streams, additional process variables, and auxiliary measurements to be communicated.

What Is an Industrial Physical Layer Device (PHY)?
An Industrial Ethernet PHY is a physical layer transceiver device for sending and receiving Ethernet frames based on the OSI network model. In the OSI model, Ethernet covers Layer 1 (the physical layer) and part of Layer 2 (the data link layer) and is defined by the IEEE 802.3 standard. The physical layer specifies the types of electrical signals, signaling speeds, media and connector types, and network topologies. It implements the Ethernet physical layer portion of the 1000BASE-T (1000 Mbps), 100BASE-TX (100 Mbps over copper), and 10BASE-T (10 Mbps) standards.
The data link layer specifies how communications occur over the media as well as the frame structure of messages transmitted and received. This simply means how the bits come off the wire and into a bit arrangement so the data can be extracted from the bit stream. For Ethernet, this is called media access control, or MAC for short.
Key Considerations When Selecting an Industrial PHY
Performance
The network cycle time is the communication time required by the controller to both collect and update the data memories of all devices. A low latency PHY reduces network cycle time, improving network refresh time and allowing more devices to be connected to the network.
Robustness
Built to withstand external radiated and conducted noise sources given the harsh operating environment. Select products have been tested and adhere to EMI/EMC standards like CISPR 32 and IEC 61000-4-2 through IEC 6100-4-6. This robustness helps prevent lengthy redesign cycles to secure certification later in the development flow.
Low Power
Devices for industrial applications are typically IP65/IP66 sealed from dust and moisture and, hence, have restricted airflow and limited power dissipation capability. Similarly, these devices are often exposed to high ambient temperature in industrial environments. Because line and ring topologies require two ports and two PHYs, power dissipation is doubled for data in and out.
Featured Technical Articles

Robust Ethernet Physical Layer Solutions for Time Critical Communications in Harsh Industrial Environments

Enabling Seamless Ethernet to the Field with 10BASE-T1L Connectivity
Product Highlights

Ethernet to the Edge with 10BASE-T1L

Lowest Latency, Gigabit, Industrial Ethernet PHY
Latest Resources
Technical Articles
-
Ethernet-APL: Optimization of Process Automation with Actionable Insights
Thought Leadership
- Designing a Deployable 10BASE-T1L Single-Pair Ethernet Condition Monitoring Vibration Sensor
-
10BASE-T1L: Extending the Scope for Big Data Analytics to the Edge of the Factory Network
Thought Leadership
- What Matters When It Comes to Choosing an Ethernet PHY
- The New 10BASE-T1L Standard—Has Anything Changed?
Application Notes
Solutions Bulletins & Brochures
Webcasts
- NEW Reduce System Development Time, TTM and Risk with the Latest Multiprotocol Industrial Ethernet Switch Platform Webinar (EngineerZone)
- Technologies Enabling the Future of Intelligent Field Devices Webinar (EngineerZone)
- 10Base-T1 System Design Considerations (EngineerZone)
- Designing Industrial Connectivity Solutions for The Smart Factory
- Spread the Word: This Is the Power of Silence
Videos
- Enable Sustainable Manufacturing with Variable Speed Drive Solutions
- Sustainability through Ethernet Connected Building Controllers
- Enable Sustainable Enterprises of the Future with Ethernet Connected Building Controllers
- Elevate Surveillance with Cameras that See, Sense and Think
- Sensors Converge 2022, Empowering the Intelligent Edge