ADI Semiconductor Automatic Test Equipment Solution
Test for semiconductor IC components can usually be divided into CP (chip probe) at the wafer level and the final package test (FT). The main difference between these two is that the CP is a functional test for the die before packaging, while the FT is an IC specification test after packaging. The purpose of the die test is mainly to avoid problems found during the FT test and an even heavier burden to cost while improving product passed yield. The integrated circuit test (IC test) is implemented mainly to distinguish qualified ICs from unqualified ones and ensure the final product specification, quality, and reliability. With the rapid development of integrated circuits, the scale of the semiconductor test market has become larger and larger. The growing test market has led to higher requirements for circuit quality and reliability.
Fill Out the Form Below to Get Your Multichannel Source Measurement Unit (SMU) Solution PDF

About Analog Devices
Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index.