Gigabit Digital Isolators for Video, Converters, Communications

Various reports indicate that the digital isolation market will grow at over 6% per year, for the next 5 years. This growth coupled with faster communication speeds, in excess of 1Gbps, is reshaping many markets and applications. In this webcast, we will discuss the requirements for isolation of high-speed links in medical, instrumentation, industrial, motor control and robotics applications.
View Webcast
( Registration required )

Dr. Conal Watterson is an applications engineer in the Interface and iCoupler® Digital Isolator Group at Analog Devices in Limerick, Ireland. A Ph.D. and M. Eng. graduate of the University of Limerick since 2010, Conal has published a number of papers and articles on industrial fieldbus networks, diagnostics/reliability and high-speed signaling and isolation. His current focus topics are high-speed interfaces & isolators and universal serial bus (USB).