Education Library

Frequently Asked Question

Are all digital potentiometers limited to |5V|?

No. The AD7376 and AD5290 handle ±15V or single +30V. The AD5260/5262/5280/5282/5263 all handle ±5V or single +12V. The remaining ones are limited to |5V|.