Introduction
The AD8494/AD8495/AD8496/AD8497 thermocouple amplifiers provide a simple, low cost solution for measuring thermocouple temperatures. These amplifiers simplify many of the difficulties of measuring thermocouples. A fixed-gain instrumentation amplifier amplifies the small thermocouple voltage, and an integrated temperature sensor performs cold junction compensation.
The AD849x is optimized to measure and amplify J and K type thermocouple signals for a linear 5 mV/°C response such that

where TMJ is the temperature at the measurement junction of the thermocouple.
The AD849x output is accurate to within 2°C across the entire range of measurement and ambient temperatures listed in Table 1 This application note describes ways to achieve even greater accuracy when operating at or measuring temperatures outside the specified ranges using the AD849x.
Thermocouple Nonlinearity
The voltage generated by a thermocouple is inherently nonlinear. For example, a J type thermocouple changes by 52 μV/°C at 25°C and by 55 μV/°C at 150°C. K type thermocouples tend to be much more linear, staying fairly near 41 μV/°C when temperatures are above 0°C. The voltage response of a thermocouple to a temper ture gradient can be described by a greater than sixth-order polynomial (see Figure 1).

Figure 1. Seebeck Coefficient of Thermocouple vs. Temperature
The AD849x linearly amplifies the (cold junction compensate thermocouple signal. This means that the output signal is as d) nonlinear as the input signal from the thermocouple.
An application may require better nonlinearity (meaning greater accuracy) than is provided directly by the thermocouple in that temperature range. In such cases, linearization, or correction, of the thermocouple measurement is required.
Whether a thermocouple measurement needs linearization depends on the type of thermocouple chosen, the required system accuracy, and the temperature range being measured. The nonlinearity of thermocouple signals is well studied and is constant for a specific thermocouple type. Therefore, the measurement system can compensate for it.
AD849x Thermocouple Nonlinearity Compensation
Although the AD849x does not actively correct thermocouple nonlinearity, the amplifiers are precision trimmed to match the transfer characteristics of J type and K type thermocouples. This means that the AD849x compensates for nonlinearity by choosing a specific section of the thermocouple curve and performing a linear best fit to this section to create a 5 mV°/C output.
Table 1 shows the temperature ranges chosen, resulting in an error from thermocouple nonlinearity of less than ±2°C. Figure 2 shows the nonlinearity error graphically.
Part | Thermocouple Type | Max Error | Ambient Temperature Range | Measurement Temperature Range |
AD8494 | J | ±2°C | 0°C to 50°C | −35°C to +95°C |
AD8495 | K | ±2°C | 0°C to 50°C | −25°C to +400°C |
AD8496 | J | ±2°C | 25°C to 100°C | +55°C to +565°C |
AD8497 | K | ±2°C | 25°C to 100°C | −25°C to +295°C |

Figure 2. AD849x Output Error due to Thermocouple Nonlinearity
Each part in the AD849x family is precision trimmed to optimize a linear operating range for a specific thermocouple type and for specific measurement and ambient temperature ranges. The following three parameters are trimmed to achieve a 5 mV/°C output with minimal errors:
- Gain of the amplifier
- Offset of the amplifier (error voltage at 0°C to achieve 125 mV at 25°C)
- Scale factor of the temperature sensor/cold junction compensator
The thermocouple voltage, VTC, is a function of the thermocouple type, the measurement junction temperature (TMJ), and the reference junction temperature (TRJ).

The following transfer function should be used to determine the actual thermocouple voltages being measured by the AD849x (see Table 2 for specific values for each part).

where:
CJC is the cold junction compensation scale factor.
VOFFSET is the error voltage at 0°C to achieve 125 mV at 25°C.
VREF is the user input voltage.
Gain is the gain of the amplifier.
Part | Gain | CJC Factor (mV/°C) | Offset (mV) |
AD8494 | 96.7 | 5 | 0 |
AD8495 | 122.4 | 4.95 | 1.25 |
AD8496 | 90.35 | 4.8 | 20.2 |
AD8497 | 122.4 | 5.0392 | −0.98 |
Linearity Correction Algorithms
Thermocouple nonlinearity is typically corrected with a microcontroller in the digital domain. One of two correction algorithms can be used.
AD849x Output Lookup Table
The first method is to use Table 3, which lists the ideal AD849x output voltages as a function of the temperature for J type and K type thermocouples with the specified junction temperatures.
For example, an AD8495 at room temperature (25°C) with a grounded reference pin connected to a K type thermocouple outputs 1 V. Using the 5 mV/°C transfer function, 1 V represents 200°C. For greater accuracy, the user must calculate the temperature that corresponds to the 1 V output as follows:
- Table 3 indicates that at a measurement junction temperature of 200°C, the actual AD8495 output is 0.999 V, and at a measurement junction temperature of 220°C, it is 1.097 V.
- Linear extrapolation between these two points yields an answer of 200.2°C at 1 V.
NIST Thermoelectric Voltage Lookup Tables
The second method is to use the following equations, where TMJ is the temperature at the thermocouple measurement junction, and fNIST is a millivolt-to-temperature function based on the standard lookup tables or on equations published by the National Institute of Standards and Technology (thermocouple databases can be found at http://srdata.nist.gov/its90/main).
Recall that VTC ∝ TMJ − TRJ, such that

Output values for intermediate temperatures can be interpolated or calculated using the AD849x output equations and the NIST thermoelectric voltage tables referred to 0°C.
For the AD8494, the equation is as follows:

For the AD8495, the equation is as follows:

For the AD8496, the equation is as follows:

For the AD8497, the equation is as follows:

Using the same example as for the first method (an AD8495 at room temperature with a grounded reference pin connected to a K type thermocouple that reads 1 V), the correction procedure is as follows:

- Consulting a standard K type thermocouple table indicates that at a measurement junction temperature of 200°C, the thermoelectric voltage of the thermocouple is 8.138 mV, and at a measurement junction temperature of 201°C, the thermoelectric voltage is 8.178 mV.
- Linear extrapolation yields a final answer of 200.5°C.
Measurement Junction Temperature (°C) | AD8494/AD8495 Output, TA = TRJ = 25°C | AD8496/AD8497 Output, TA = TRJ = 60° | ||||
Ideal Output (V) | Actual Output (V) | Ideal Output (V) | Actual Output (V) | |||
AD8494/AD8495 | AD8494 Output with J Type | AD8495 Output with K Type | AD8496/AD8497 | AD8496 Output with J Type | AD8497 Output with K Type | |
−260 | −1.3 | −0.786 | −1.3 | −0.785 | ||
−240 | −1.2 | −0.774 | −1.2 | −0.773 | ||
−220 | −1.1 | −0.751 | −1.1 | −0.751 | ||
−200 | −1 | −0.719 | −1 | −0.718 | ||
−180 | −0.9 | −0.714 | −0.677 | −0.9 | −0.642 | −0.676 |
−160 | −0.8 | −0.658 | −0.627 | −0.8 | −0.590 | −0.626 |
−140 | −0.7 | −0.594 | −0.569 | −0.7 | −0.530 | −0.568 |
−120 | −0.6 | −0.523 | −0.504 | −0.6 | −0.464 | −0.503 |
−100 | −0.5 | −0.446 | −0.432 | −0.5 | −0.392 | −0.432 |
−80 | −0.4 | −0.365 | −0.355 | −0.4 | −0.315 | −0.354 |
−60 | −0.3 | −0.278 | −0.272 | −0.3 | −0.235 | −0.271 |
−40 | −0.2 | −0.188 | −0.184 | −0.2 | −0.150 | −0.184 |
−20 | −0.1 | −0.095 | −0.093 | −0.1 | −0.063 | −0.092 |
0 | 0 | 0.002 | 0.003 | 0 | 0.027 | 0.003 |
20 | 0.1 | 0.100 | 0.100 | 0.1 | 0.119 | 0.101 |
25 | 0.125 | 0.125 | 0.125 | 0.125 | 0.142 | 0.126 |
40 | 0.2 | 0.201 | 0.200 | 0.2 | 0.213 | 0.200 |
60 | 0.3 | 0.303 | 0.301 | 0.3 | 0.308 | 0.301 |
80 | 0.4 | 0.406 | 0.402 | 0.4 | 0.405 | 0.403 |
100 | 0.5 | 0.511 | 0.504 | 0.5 | 0.503 | 0.505 |
120 | 0.6 | 0.617 | 0.605 | 0.6 | 0.601 | 0.605 |
140 | 0.7 | 0.723 | 0.705 | 0.7 | 0.701 | 0.705 |
160 | 0.8 | 0.829 | 0.803 | 0.8 | 0.800 | 0.804 |
180 | 0.9 | 0.937 | 0.901 | 0.9 | 0.900 | 0.902 |
200 | 1 | 1.044 | 0.999 | 1 | 1.001 | 0.999 |
220 | 1.1 | 1.151 | 1.097 | 1.1 | 1.101 | 1.097 |
240 | 1.2 | 1.259 | 1.196 | 1.2 | 1.201 | 1.196 |
260 | 1.3 | 1.366 | 1.295 | 1.3 | 1.302 | 1.296 |
280 | 1.4 | 1.473 | 1.396 | 1.4 | 1.402 | 1.396 |
300 | 1.5 | 1.580 | 1.497 | 1.5 | 1.502 | 1.498 |
320 | 1.6 | 1.687 | 1.599 | 1.6 | 1.602 | 1.599 |
340 | 1.7 | 1.794 | 1.701 | 1.7 | 1.702 | 1.701 |
360 | 1.8 | 1.901 | 1.803 | 1.8 | 1.801 | 1.804 |
380 | 1.9 | 2.008 | 1.906 | 1.9 | 1.901 | 1.907 |
400 | 2 | 2.114 | 2.010 | 2 | 2.001 | 2.010 |
420 | 2.1 | 2.221 | 2.113 | 2.1 | 2.100 | 2.114 |
440 | 2.2 | 2.328 | 2.217 | 2.2 | 2.200 | 2.218 |
460 | 2.3 | 2.435 | 2.321 | 2.3 | 2.300 | 2.322 |
480 | 2.4 | 2.542 | 2.425 | 2.4 | 2.401 | 2.426 |
500 | 2.5 | 2.650 | 2.529 | 2.5 | 2.502 | 2.530 |
520 | 2.6 | 2.759 | 2.634 | 2.6 | 2.603 | 2.634 |
540 | 2.7 | 2.868 | 2.738 | 2.7 | 2.705 | 2.739 |
560 | 2.8 | 2.979 | 2.843 | 2.8 | 2.808 | 2.843 |
580 | 2.9 | 3.090 | 2.947 | 2.9 | 2.912 | 2.948 |
600 | 3 | 3.203 | 3.051 | 3 | 3.017 | 3.052 |
620 | 3.1 | 3.316 | 3.155 | 3.1 | 3.124 | 3.156 |
640 | 3.2 | 3.431 | 3.259 | 3.2 | 3.231 | 3.259 |
660 | 3.3 | 3.548 | 3.362 | 3.3 | 3.340 | 3.363 |
680 | 3.4 | 3.666 | 3.465 | 3.4 | 3.451 | 3.466 |
700 | 3.5 | 3.786 | 3.568 | 3.5 | 3.562 | 3.569 |
720 | 3.6 | 3.906 | 3.670 | 3.6 | 3.675 | 3.671 |
740 | 3.7 | 4.029 | 3.772 | 3.7 | 3.789 | 3.773 |
760 | 3.8 | 4.152 | 3.874 | 3.8 | 3.904 | 3.874 |
780 | 3.9 | 4.276 | 3.975 | 3.9 | 4.020 | 3.976 |
800 | 4 | 4.401 | 4.076 | 4 | 4.137 | 4.076 |
820 | 4.1 | 4.526 | 4.176 | 4.1 | 4.254 | 4.176 |
840 | 4.2 | text-align: center;4.650 | 4.275 | 4.2 | 4.370 | 4.276 |
860 | 4.3 | 4.774 | 4.374 | 4.3 | 4.486 | 4.375 |
880 | 4.4 | 4.897 | 4.473 | 4.4 | 4.600 | 4.474 |
900 | 4.5 | 5.018 | 4.571 | 4.5 | 4.714 | 4.572 |
920 | 4.6 | 5.138 | 4.669 | 4.6 | 4.826 | 4.670 |
940 | 4.7 | 5.257 | 4.766 | 4.7 | 4.937 | 4.767 |
960 | 4.8 | 5.374 | 4.863 | 4.8 | 5.047 | 4.863 |
980 | 4.9 | 5.490 | 4.959 | 4.9 | 5.155 | 4.960 |
1000 | 5 | 5.606 | 5.055 | 5 | 5.263 | 5.055 |
1020 | 5.1 | 5.720 | 5.150 | 5.1 | 5.369 | 5.151 |
1040 | 5.2 | 5.833 | 5.245 | 5.2 | 5.475 | 5.245s |
1060 | 5.3 | 5.946 | 5.339 | 5.3 | 5.581 | 5.339 |
1080 | 5.4 | 6.058 | 5.432 | 5.4 | 5.686 | 5.433 |
1100 | 5.5 | 6.170 | 5.525 | 5.5 | 5.790 | 5.526 |
1120 | 5.6 | 6.282 | 5.617 | 5.6 | 5.895 | 5.618 |
1140 | 5.7 | 6.394 | 5.709 | 5.7 | 5.999 | 5.710 |
1160 | 5.8 | 6.505 | 5.800 | 5.8 | 6.103 | 5.801 |
1180 | 5.9 | 6.616 | 5.891 | 5.9 | 6.207 | 5.891 |
1200 | 6 | 6.727 | 5.980 | 6 | 6.311 | 5.981 |
1220 | 6.1 | 6.069 | 6.1 | 6.070 | ||
1240 | 6.2 | 6.158 | 6.2 | 6.158 | ||
1260 | 6.3 | 6.245 | 6.3 | 6.246 | ||
1280 | 6.4 | 6.332 | 6.4 | 6.332 | ||
1300 | 6.5 | 6.418 | 6.5 | 6.418 | ||
1320 | 6.6 | 6.503 | 6.6 | 6.503 | ||
1340 | 6.7 | 6.587 | 6.7 | 6.588 | ||
1360 | 6.8 | 6.671 | 6.8 | 6.671 | ||
1380 | 6.9 | 6.754 | 6.9 | 6.754 |