Highly Integrated 2.5A Backup Power Manager Provides High Efficiency Charging & System Backup for up to Two Supercapacitors

Jul 31 2018 - Norwood, MA
  • LTC4041Analog Devices announces the Power by Linear LTC4041, a complete supercapacitor backup power management system for 2.9V to 5.5V supply rails that must be kept active during a main power failure. Supercapacitors have higher power density than batteries, making them ideal for systems requiring high peak power backup for short periods of time.



    The LTC4041 uses an on-chip bidirectional synchronous converter to provide high efficiency step-down supercapacitor charging, as well as high current, high efficiency boost backup power. When external power is available, the device operates as a step-down battery charger for one or two supercapacitor cells while giving preference to the system load. When the input supply drops below the adjustable power-fail input (PFI) threshold, the LTC4041 switches to step-up regulator operation, capable of delivering up to 2.5A to the system load from the supercapacitor. During a power fail event, the device’s PowerPath™ control provides reverse blocking and a seamless switchover from input power to backup power. Typical applications for the LTC4041 include ride-through “dying gasp” supplies, high current ride-through 3V-5V uninterruptible power supplies (UPSs), power meters, industrial alarms, servers and solid-state drives.


    The LTC4041 includes an optional overvoltage protection (OVP) function using an external FET which can protect the IC from input voltages greater than 60V. An internal supercapacitor balancing circuit maintains equal voltages across each supercapacitor and limits the maximum voltage of each supercapacitor to a predetermined value. Its adjustable input current limit function enables operation from a current limited source while prioritizing system load current over battery charge current. An external disconnect switch isolates the primary input supply from the system during backup. The device also includes input current monitoring, an input power fail indicator, and a system power fail indicator.


    The LTC4041 is offered in a low profile (0.75mm) 24-lead 4mm x 5mm QFN package with backside metal pad for excellent thermal performance. The device operates from –40°C to 125°C, in both E and I grades. For more information, visit www.analog.com/LTC4041.


    Summary of Features: LTC4041


    • 2.5A Step-Down Supercapacitor Charger & 2.5A Step-Up Backup Supply
    • 6.5A Switches for 2.5A Backup from One Supercapacitor or Two in Series
    • Input Current Limit Prioritizes Load over Charge Current
    • Input Ideal Diode Isolates Input During Backup
    • Automatic Seamless Switchover to Backup Mode
    • Internal Supercapacitor Balancer (No External Resistors)
    • Programmable Charge Current & Charge Voltage
    • Input Power Fail Indicator
    • System Power Good Indicator
    • Optional OVP Circuitry Protects Device to >60V
    • Constant Frequency Operation
    • Thermally Enhanced 24-Lead 4mm × 5mm QFN Package

    Pricing & Availability

    Product Production Availability Price Each per 1,000 Packaging
    LTC4041EUFD#PBF Now Starts at $2.90 24-Lead 4mm x 5mm QFN
    LTC4041IUFD#PBF Now Starts at $3.30 24-Lead 4mm x 5mm QFN


  • About Analog Devices
  • Analog Devices (Nasdaq: ADI) is a leading global high-performance analog technology company dedicated to solving the toughest engineering challenges. We enable our customers to interpret the world around us by intelligently bridging the physical and digital with unmatched technologies that sense, measure, power, connect and interpret. Visit http://www.analog.com
  • Subscribe to Analog Dialogue, ADI’s monthly technical journal, at: http://www.analog.com/library/analogDialogue/


    All registered trademarks and trademarks are the property of their respective owners.

  • Editor's Contact Information
Stay Informed