150VIN & VOUT Synchronous 4-Switch Buck-Boost Controller with Integrated Switching Bias Supply

Feb 12 2018 - MILPITAS, CA
  • NORWOOD, MA – February 12, 2018 – Analog Devices announces the Power by Linear LTC3777, a 150V high efficiency (up to 99%) 4-switch synchronous buck-boost DC/DC controller, which operates from input voltages above, below or equal to the regulated output voltage. Its 4.5V to 150V input voltage range operates from a high input voltage source or from an input that has high voltage surges, eliminating the need for external surge suppression devices, ideal for transportation, industrial and medical applications.


     

    To prevent high on-chip power dissipation in high input voltage applications, the LTC3777 integrates a low quiescent current high efficiency switching bias supply for its internal power consumption. The output voltage of the LTC3777 can be set from 1.2V to 150V at output currents up to tens of amps, depending on the choice of external components. Output power up to 500W can be delivered with a single device. Higher powers can be achieved when multiple circuits are configured in parallel. The LTC3777's powerful 1.5Ω N-channel MOSFET gate drivers can be adjusted from 6V to 10V, enabling the use of logic-level or standard-threshold MOSFETs.

    The LTC3777 employs a proprietary current mode control architecture for constant frequency in buck, boost or buck-boost modes. The operating frequency can be synchronized to an external clock from 50kHz to 600kHz, while an input/output constant current loop provides support for battery charging and overload protection. The user can select either forced continuous mode or discontinuous mode to maximize light load efficiency. Additional features include seamless transfers between operating regions, a power good output voltage monitor, adjustable soft-start and input overvoltage lockout, and output voltage disconnect during shutdown.

    The LTC3777 is available in a 48-lead e-LQFP package with pin skipping for high voltage spacing. Extended and industrial versions are available from –40 to 125°C. For more information, go to www.linear.com/product/LTC3777.


    Summary of Features: LTC3777

    • 4-Switch Synchronous Current Mode Buck-Boost Architecture
    • Operation with Input Voltages Above, Below or Equal to the Output Voltage
    • 4.5V to 150V Input Voltage Range
    • 1.2V to 150V Output Voltage Range
    • Up to 99% Efficiency
    • Integrated Switching Bias Supply
    • Input or Output Average Current Limit
    • Adjustable 6V to 10V MOSFET Gate Drivers
    • Compatible with Logic-Level or Standard-Threshold NMOS
    • 500 Watts Output Power Capable with a Single Device
    • Fixed Synchronizable Operating Frequency from 50kHz to 600kHz
    • Output Voltage Disconnect from VIN During Shutdown
    • Adjustable Soft-Start
    • ±1% Reference Voltage Accuracy over -40°C to 125°C
    • 48-Lead e-LQFP Package with High Voltage Pin Skipping

    Pricing & Availability

    Product Sample Availability Production Availability Price Each Per 1,000 Package
    LTC3777 Now Now Starts at $8.40 e-LQFP-48 7mm × 7mm

     

    About Analog Devices

    Analog Devices is the leading global high-performance analog technology company dedicated to solving the toughest engineering challenges. We enable our customers to interpret the world around us by intelligently bridging the physical and digital with unmatched technologies that sense, measure, power, connect and interpret. Visit http://www.analog.com.

    Follow ADI on Twitter at http://www.twitter.com/ADI_News

    Subscribe to Analog Dialogue, ADI’s monthly technical journal, at:
    http://www.analog.com/library/analogDialogue/

    All registered trademarks and trademarks are the property of their respective owners.


    Contacts:

    John Hamburger
    Analog Devices, Inc.
    john.hamburger@analog.com
    Tel: 408-432-1900 ext 2419

    Doug Dickinson
    Analog Devices, Inc.
    douglas.dickinson@analog.com
    Tel: 408-432-1900 ext 2233


    Download Word Version

    Download PDF Version

  • About Analog Devices
  • Analog Devices (Nasdaq: ADI) is a leading global high-performance analog technology company dedicated to solving the toughest engineering challenges. We enable our customers to interpret the world around us by intelligently bridging the physical and digital with unmatched technologies that sense, measure, power, connect and interpret. Visit http://www.analog.com
Stay Informed