Transceiver Provides Reliable Radio Connections and Extended Battery Life for IoT and Other Wireless Applications

Jun 22 2016 -Norwood, MA
  • ADF7030-1-PR-Title-Web

    Analog Devices, Inc. (ADI) today introduced a low power, high performance, radio transceiver for battery powered applications. The new transceiver enables more reliable wireless radio connections with fewer retries and packet losses as well as longer battery lifetime. The ADF7030-1 features a highly sensitive receiver and superior immunity to signal interferences as well as low power modes, including the industry’s lowest current in sleep mode. Designed with ADI’s advanced radio technology, the transceiver is ideal for users of Internet of Things (IoT) devices, smart metering, security and building automation, industrial control, and wireless sensor networks.


    The new ADF7030-1 sub-GHz integrated radio transceiver supports narrowband and wideband operation across sub-GHz ISM bands and data rates from 0.1 kbps to 300 kbps using 2GFSK modulation. The radio transceiver also supports Wireless M-Bus (WMBUS) and IEEE 802.15.4g-based protocols. Offering excellent receiver sensitivity that maximizes link budgets and support for larger cell sizes with a high immunity to interference, the new transceiver also improves system reliability. The ADF7030-1 transceiver features a smart wake mode that provides low overall power consumption enabling long lifetime in battery operated systems while maintaining excellent RF performance. The device can enter a low power sleep mode consuming only 10 nA with memory retained.

    With an emphasis on flexibility and ease of use, the ADF7030-1 radio transceiver features an on-chip ARM® Cortex®-M0 radio processor that performs radio control and calibration, including time sequencing that reduces engineering development time. A highly programmable packet handler saves more valuable time by simplifying programming interfaces and code development on the host microprocessor. Comprehensive testing by ADI allows engineers to deploy network settings confidently without spending additional time optimizing settings to maximize performance.

    Pricing and Availability
    Product Product Availability Price Each per 1000 Description
    ADF7030-1BCPZN Now $1.99 6 mm × 6 mm, 40-lead, LFCSP
    ADF70301-868EZKIT July 1 unit @ $599.00 Evaluation and Development Kit
    ADF70301-433EZKIT July 1 unit @ $599.00 Evaluation and Development Kit
    ADF70301-169EZKIT July 1 unit @ $599.00 Evaluation and Development Ki

     

  • About Analog Devices
  • Analog Devices (NASDAQ: ADI) designs and manufactures semiconductor products and solutions. We enable our customers to interpret the world around us by intelligently bridging the physical and digital with unmatched technologies that sense, measure and connect. Visit http://www.analog.com
  • EngineerZone is a registered trademark of Analog Devices, Inc. All other trademarks are the property of their respective owners.

    Read and subscribe to Analog Dialogue, ADI’s monthly technical journal, at: http://www.analog.com/library/analogDialogue/

  • Editor's Contact Information
Stay Informed