Analog Devices’ MEMS Accelerometers Enable Early Detection of Structural Defects
Analog Devices, Inc. (ADI) today announced three-axis, MEMS accelerometers that perform high resolution vibration measurement with very low noise to enable the early detection of structural defects via wireless sensor networks. The low power consumption of the new ADXL354 and ADXL355 accelerometers lengthens battery life and allows extended product usage by reducing the time between battery changes. The low noise performance of the ADXL354 and ADXL355 with low power consumption makes it now possible to cost-effectively enable low-level vibration measurement applications such as Structural Health Monitoring (SHM). Additionally, the tilt stability of ADXL354 and ADXL355 accelerometers delivers excellent repeatability over temperature and time, which is ideal for orientation and navigation systems in unmanned aerial vehicles using Inertial Measurement Units (IMUs) and inclinometers. By providing repeatable tilt measurement under all conditions, the new accelerometers enable minimal tilt error without extensive calibration in harsh environments.
- View the ADXL354 product page, download data sheet, order samples and evaluation boards: http://www.analog.com/ADXL354
- View the ADXL355 product page, download data sheet, order samples and evaluation boards: http://www.analog.com/ADXL355
The ADXL354 and ADXL355 accelerometers offer guaranteed temperature stability with null offset coefficients of 0.15mg/C (max). The stability minimizes resource and expense associated with calibration and testing effort, helping to achieve higher throughput for device OEMs. In addition, the hermetic package helps ensure that the end product conforms to its repeatability and stability specifications long after they leave the factory.
With output of ±2g to ±8g full scale range (FSR), selectable digital filtering from 1 Hz to 1 kHz, and low noise density of 25µ/√Hz at less than 200µA current consumption, the ADXL354 and ADXL355 accelerometers offer performance level comparable to much more expensive devices with less power consumption and BOM cost.
Product Pricing and Availability
Product Output Interface Sample Availability Full Production Price Each per 1,000 Packaging ADXL354 Analog Now Now $25.42 6x6 mm 14-lead LCC ADXL355 SPI Now Now $28.25 6x6 mm 14-lead LCC - About Analog Devices
- Analog Devices (NASDAQ: ADI) designs and manufactures semiconductor products and solutions. We enable our customers to interpret the world around us by intelligently bridging the physical and digital with unmatched technologies that sense, measure and connect. Visit http://www.analog.com
-
EngineerZone is a registered trademark of Analog Devices, Inc.
Read and subscribe to Analog Dialogue, ADI’s monthly technical journal, at: http://www.analog.com/library/analogDialogue/
-
Editor's Contact Information
-
Linda Kincaid
Global PR Manager
linda.kincaid@analog.com
-
Linda Kincaid