Analog Devices Introduces Industry’s First Analog Fault Detection and Protection Switch Family for Analog Input/Output Modules in Harsh Environments
Analog Devices, Inc. (NASDAQ: ADI) today introduced a family of fault detection and protection, low/ultra-flat Ron switches: the ADG5412F, ADG5413F, ADG5412BF and ADG5413BF. By identifying when a channel is in a fault, this innovative switch technology removes the need for additional hardware and software error-detection schemes, leading to an improvement in system uptime.
The new switches also offer a best-in-class combination of robustness and precision performance in a small package, suiting them for precision instrumentation, process control and avionic signal chains. Providing up to ± 55-V over-voltage protection, coupled with a 5.5-kV HBM ESD level, these switches protect downstream system components in both power-on and power-off states, while protecting against hot-swapping and operator miss-use events. The leading-edge combination of low Ron, Ron flatness and low leakage, coupled with the removal of discrete protection components, leads to a reduction in signal distortion and system error budget. The ultra-low Ron flatness level offered by this family also minimizes system total harmonic distortion and noise performance.
- Download ADG5412F quad single-pole/single-throw (SPST) switches data sheet, view product page and order samples
- Download ADG5412BF bi-directional fault protection and detection, quad SPST switches data sheet, view product page and order samples
- Download ADI’s switches and muxes portfolio
Key Features:
- Over-voltage detection on source pins
- Over-voltage protection up to −55 V and +55 V
- Bi-directional over-voltage protection (ADG5412BF / ADG5413BF)
- Low on-resistance of 10 Ω, on-resistance flatness of 0.5 Ω
- VSS to VDD analog signal range
- ±5-V to ±22-V dual-supply operation
- 8-V to 44-V single-supply operation
- Fully specified at ±15 V, ±20 V, +12 V, and +36 V
Pricing and Availability Product Production Availability Configuration Option Operating Temperature Range Packaging Price Each In 1,000 Quantities ADG5412F NOW Quad SPST
Logic 1 On-40°C to +125°C 16-lead TSSOP $3.96 ADG5413F NOW Quad SPST
2* Logic 1 On
2* Logic 0 On-40°C to +125°C 16-lead TSSOP $3.96 ADG5412BF NOW Bi-directional OVP
Quad SPST
Logic 1 On-40°C to +125°C 16-lead TSSOP $3.96 ADG5413BF NOW Bidirectional OVP
Quad SPST
2* Logic 1 On
2* Logic 0 On-40°C to +125°C 16-lead TSSOP $3.96 ADG5412F, ADG5413F,
ADG5412BF,ADG5413BFSAMPLING NOW As Above -40°C to +125°C 16-Lead 4×4mm LFCSP $3.96 ADG5404F SAMPLING NOW 4:1 Mux -40°C to +125°C 16-lead TSSOP $3.86 More About ADI’s Analog Fault Protection and Detection Switch and Multiplexor Family
The release of these switch products, along with the sampling of the ADG5404F 4:1 multiplexor, forms the start of a new ADI product portfolio designed to maximize system operation in harsh environments.
- About Analog Devices
- Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index.
-
EngineerZone is a trademark of Analog Devices, Inc.
Follow ADI on Twitter
To subscribe to Analog Dialogue, ADI's monthly technical journal, visit: http://www.analog.com/subscribe
-
Editor's Contact Information
-
Grainne Murphy
Market Manager
grainne.murphy@analog.com
-
Grainne Murphy