Analog Devices Introduces the First Integrated Analog Controller Optimizing High-Efficiency Rechargeable Battery Manufacturing

Two-device integrated analog controller is designed for battery formation and grading systems for medium- and high-energy batteries used in hybrid and electric vehicles, energy storage and industrial tools.

Oct 28 2014 - Norwood, MA
  • Battery_Testing_PRAnalog Devices, Inc. (NASDAQ: ADI) today introduced two components that work together as an integrated analog controller to offer energy recycling and significant performance and cost benefits over current rechargeable battery formation and grading system solutions. The AD8450/1 precision analog front-end and controller, and the ADP1972 buck or boost PWM controller provide energy efficiency benefits in the charging and discharging cycles, both as the current is provided through a PWM controller as well as when it is directed back to the grid or to charge other cells.

    Unique to this two-device architecture is the use of analog control loops, which offer significant benefits over the current digital solution. These benefits include faster control of up to 1.5 MHz for the critical signal path, greater than 90 percent efficiency and higher accuracy over temperature. The solution is designed for battery formation and grading systems for medium- and high-energy batteries used in hybrid and electric vehicles, energy storage and industrial tools.

    • Download the precision analog front-end and controller data sheet, view product page and order samples
    • Download the buck or boost PWM controller data sheet, view product page and order samples
    • Learn more about battery test and formatting

    Other benefits of this system solution include the ability to share lower-cost precision D/A converters and A/D converters over multiple channels. This reduces overall system cost and the size of the surrounding power components while improving the capability of switching frequencies up to 300 kHz. The addition of synchronization with phase-shifting between channels reduces input filtering. Also, the solution minimizes the need for complex coding and cuts system calibration time in half. Both synchronous and non-synchronous architectures are available. Design tools and total reference designs are provided for customers to minimize development cost and cycle.

    Pricing and Availability
    Product Samples and
    Production
    Availability
    Operating
    Temperature Range
    Price each
    per 1K
    Packaging
    AD8450
    NOW –40° C to +85° C
    $6.95
    80-lead LQFP
    AD8451
    NOW
    –40° C to +85° C
    $5.40
    80-lead LQFP
    ADP1972
    NOW
    –40°C to +125°C
    $3.50
    16-Lead TSSOP

     

  • About Analog Devices
  • Innovation, performance, and excellence are the cultural pillars on which Analog Devices has built one of the longest standing, highest growth companies within the technology sector. Acknowledged industry-wide as the world leader in data conversion and signal conditioning technology, Analog Devices serves over 60,000 customers, representing virtually all types of electronic equipment. Analog Devices is headquartered in Norwood, Massachusetts, with design and manufacturing facilities throughout the world. Analog Devices is included in the S&P 500 Index.
  • EngineerZone is a trademark of Analog Devices, Inc.

    To subscribe to Analog Dialogue, ADI's monthly technical journal, visit: http://www.analog.com/subscribe

  • Editor's Contact Information
Stay Informed