Keyboard Shortcuts

Keyboard shortcuts are an alternate way to invoke one or more commands in LTspice that would otherwise only be accessible by clicking through the menu or toolbar. You can view these shortcuts for the schematic editor by choosing:

Tools > Control Panel > Drafting Options and clicking Hot Keys.

LTspice IV: Keyboard Shortcuts

Hot Keys can be reprogrammed by selecting a command and then pressing the key or key combination for the command. For example, you may want to reprogram the Undo, Redo and Duplicate (Copy) commands to a more traditional key combination. To remove a shortcut, select the command and press Delete.

Additional Hot Keys are also available for the Waveform Viewer, Symbol Editor and Netlist Editor.

For a complete reference table of Hot Keys, DOT commands and more you can download the LTspice Flyer at www.linear.com/LTspice or from the right side panel.

LTspice IV: Keyboard Shortcuts

作者

Gabino-Alonso

Gabino Alonso

Gabino Alonso目前是Power by Linear™部门的战略营销总监。加入ADI公司之前,Gabino在凌力尔特、德州仪器、加州理工州立大学担任过市场营销、工程、运营和讲师等多个职位。他拥有加州大学圣巴巴拉分校电子和计算机工程硕士学位。