faqs
Frequently Asked Question
What type of automatic frequency sweeping modes does each of your DDS parts support?
Please see the table below:
| Linear Sweep (defined endpoints - Ramped FSK) |
Linear Sweep (no defined endpoints) |
RAM mode (user defined) |
RAM mode No Automatic Frequency Sweep |
|
|---|---|---|---|---|
| AD9850 | Must be done by writing successive FTW to the part | |||
| AD9851 | Must be done by writing successive FTW to the part | |||
| AD9852 | Yes | Yes | Has a hold pin | |
| AD9854 | Yes | Yes | Has a hold pin | |
| AD9858 | Yes | Does not have a hold pin | ||
| AD9951 | Must be done by writing successive FTW to the part | |||
| AD9952 | Must be done by writing successive FTW to the part | |||
| AD9953 | Yes | |||
| AD9954 | Yes | Yes |