概览

优势和特点

  • 生命体征监测平台
  • 可穿戴电池供电平台
  • 实时数据视图
  • 数据存储到闪存,以进行离线分析
  • 轻松配置

产品详情

生命体征监测 (VSM) 手表 EVAL-HCRWATCH4Z 是模块化开发、演示和数据收集平台,适用于基于ADI公司、模拟前端 (AFE) 和传感器的高性能生命体征监测的应用。

VSM 手表是一种可穿戴的电池供电套件,可对光电容积描记 (PPG)、皮肤电活动(EDA,基于生物阻抗)、皮肤温度、心电图(ECG,基于生物电势)和运动/活动(基于 3 轴加速度计)。

VSM 手表允许在内部存储器上存储同步的多参数数据,以便以后在 PC(Windows ®操作系统)或基于 Android 或 iOS 的套件上进行数据检索和离线分析和/或实时监控。

软件

软件开发工具包

Android SDK
Android SDK provides libraries to interface with Watch platform. User application can use the SDK to receive bytes packets over a physical interface (USB or BLE) and decode it. The functionality is organized into applications, sensor manager, system functionality and algorithms. The hierarchy of objects within the SDK mirrors the applications present on the device. Each application has its own object within the SDK hierarchy, which is used to interact with the application.
Python SDK
Python SDK provides libraries to interface with Watch platform. User application can use the SDK to receive bytes packets over a physical interface (USB or BLE) and decode it. The functionality is organized into applications, sensor manager, system functionality and algorithms. The hierarchy of objects within the SDK mirrors the applications present on the device. Each application has its own object within the SDK hierarchy, which is used to interact with the application.

评估软件

ADI Study Watch (iOS)
ADI Study Watch is an app to evaluate the reference watch from Analog Devices to monitor vital signs such as PPG, ECG, Temperature, EDA measurements. The users can stream, plot the raw data from sensors real time, log the selected data in the NAND flash of the watch device for later analysis, change configuration and settings for each VSM application.
EXE
62.63 M
Wavetool Evaluation Software (Rev. 5.21.0)
A user datagram protocol (UDP) transfer capability from the Wavetool Evaluation Software allows data stream connections and register configurability to external analysis programs, such as LabVIEW® or MATLAB®, in real time.