Abstract
Application note 303 provides information on connecting the DS2151 and DS2153 single chip transceivers (SCTs) to a 16-bit DSP: the Analog Devices ADSP2181.
Interconnections between the DS2151 or DS2153 parallel port and the Analog Devices ADSP-2181 non-multiplexed I/O port are shown in Figure 1. Refer to Application Note 326: Interfacing to a Nonmultiplexed Bus for further information.
Figure 1. Transceiver - ADSP2181 Interconnections.