Rimac選擇ADI為其高性能電動汽車提供精準電池管理
2019-12-03 - 中国,台北訊
-
Terri Li
Terri.li@analog.com
Analog Devices, Inc. (ADI) 今日宣佈Rimac Automobili計畫將ADI的精準 電池管理系統 (BMS)IC應用於Rimac的BMS中,相關技術使Rimac的BMS能可靠運算任何給定時間內的電量狀態和其他電池參數,以從電池中獲取較大的電能和電量。
Rimac執行長Mate Rimac表示:「Rimac是高性能電動汽車領域的技術領導者。我們為全球眾多汽車公司開發和製造關鍵的電氣化系統,同時,我們的超級跑車也為電動汽車的性能樹立了更高標竿。我們對於BMS的要求極為嚴苛,其需實現極高的精度、極短時間內的電流和電壓劇烈變化以及在電池管理控制系統內快速動態調整。我們決定在整個電池管理系統產品線上採用ADI的電池管理IC產品組合。ADI的IC產品是我們自主研發之BMS的重要組成部分,不僅將用於我們的自有汽車上,並將應用於全球眾多汽車品牌。在針對市場上該類IC進行對比測試後,結果證實ADI的產品能夠在整個汽車生命週期內提供精準測量精度和產品可靠性。我們期待未來與ADI之合作能在我們的汽車和電池組中實現高性能BMS。」
Rimac C_Two為一款純電動超級跑車,最高時速可達412 km/h。C_Two引擎具有1,914馬力,0-96 km/h加速時間1.85秒,0-300 km/h加速時間11.8秒。為了支援高性能輸出,Rimac團隊更設計和打造包括電動傳動系統和電池組等的底層技術。
BMS技術相當於電池組背後的「大腦」,其管理輸出、充放電,並在車輛運行期間提供精準測量。BMS也透過重要的保護措施以防電池受損。電池組由多組獨立的電池單元組成,這些電池單元無縫地為汽車提供較大的電力輸出。如果電池單元之間失去均衡將會受到應力影響導致充電過早終止,進而縮短電池總體壽命。ADI的電池管理IC提供了高度精準的測量,不僅使車輛能更安全地運行,且較大化每次充電後的續航里程。
ADI汽車電氣化和資訊娛樂事業部副總裁Patrick Morgan表示:「高性能電動汽車需要高度準確的電子設備。高精準度可直接轉化為快速充電時間、較大化的電池容量和里程。我們非常高興能透過精準電池管理IC支援Rimac領先的電動汽車系統,實現全球性的優異性能。」
ADI提供廣泛的精密電池管理IC,在眾多業界應用中支援多種電池配置和電池類型。除電動汽車電池管理系統外,並包括車載充電器(OBC)、大功率電力儲存系統(ESS)、備用電池系統和高壓資料擷取系統等應用。
更多ADI電池管理解決方案請瀏覽:https://www.analog.com/en/products/power-management/battery-management/multicell-battery-stack-monitor.html
關於Rimac Automobili
Rimac Automobili由Mate Rimac於2009年成立,當時21歲的他在車庫內打造了其一輛打破吉尼斯世界紀錄的電動汽車。如今,Rimac為全球眾多汽車公司開發和製造關鍵的電氣化系統,並以自己的超級跑車為電動汽車的性能樹立新的標竿。公司總部位於克羅埃西亞札格雷布郊區,擁有約600名員工,預計將於未來實現強勁成長。Rimac垂直一體化整合了大量自主生產的元件,公司面臨的下一個挑戰是從生產複雜、高階電氣化零組件之小批量製造商成長為業界公認的一級供應商。Rimac計畫於2020年在新廠設立全新大批量生產線,以生產電池組、動力系統和C_Two超級跑車。更多Rimac Automobili資訊請瀏覽:www.rimac-automobili.com.
Forward-Looking Statements
This release may be deemed to contain forward-looking statements intended to qualify for the safe harbor from liability established by the Private Securities Litigation Reform Act of 1995. All statements other than historical facts are considered forward-looking statements, including, without limitation, statements regarding Rimac's plans to incorporate ADI's products into its electric vehicle systems. The statements contained in this press release are not guarantees of future performance, are inherently uncertain, involve certain risks, uncertainties, and assumptions that are difficult to predict. Therefore, actual outcomes and results may differ materially from what is expressed in such forward-looking statements, and such statements should not be relied upon as representing Analog Devices' expectations or beliefs as of any date subsequent to the date of this press release. Important factors that could cause actual results to differ materially from the results described, implied or projected in any forward-looking statements include Rimac's decision to use ADI as a supplier and other risk factors described in ADI's most recent filings with the Securities and Exchange Commission. We do not undertake any obligation to update forward-looking statements made by us.
Read and subscribe to Analog Dialogue, ADI's monthly technical journal, at: http://www.analog.com/analog-dialogue.html
瞭解更多在ADI工作和生活之詳細資訊請參閱:https://careers.analog.com/。
RapID™ Platform是Analog Devices, Inc的註冊商標。
關注 ADI Twitter: http://www.twitter.com/ADI_News
訂閱 ADI技術月刊 Analog Dialogue(類比對話),請參閱:http://www.analog.com/analogDialogue
ADI 台灣臉書粉絲團已經啟用,歡迎前往瀏覽、交流並按讚:https://www.facebook.com/AnalogDevicesInc.Taiwan