將A2B用於音訊會議系統

作者:ADI現場應用工程師Carlos Martins


摘要:減少會議室內的音訊線纜

如今,現代化會議室的音訊裝置面臨的主要障礙之一是需要將各種輸入/輸出感測器連接到主音訊控制台。通常是在每個節點使用單獨的點對點遮罩電纜來實現,但這種做法非常繁雜,且仍然需要在每個節點提供單獨的外部電源。除了做法繁雜之外,這些電纜並傳輸類比音訊訊號,易受明顯的頻率下降影響,特別是在長距離安裝,或者在使用經濟型電纜選項時。

適用於汽車音訊匯流排A2B®的收發器晶片透過單根非遮罩雙絞線(UTP)電纜支援多通道數位音訊。多個收發器節點可以採用菊鏈連接,除了傳輸高保真數位音訊之外,A2B匯流排還可以為由匯流排供電的遠端節點傳輸直流電源。圖1所示為A2B收發器的功能框圖。

Figure 1. An A2B functional block diagram.
圖1.A2B功能框圖。

雖然A2B收發器技術主要是為了解決汽車應用中繁雜的音訊電纜問題,但毫無疑問,它也是一種更通用的音訊廣播方法,具有廣泛的應用潛力。在汽車領域之外, A2B 技術還可用於會議室系統中。在現代會議系統中,為了實現一系列DSP功能,例如波束成型、主動降噪或回聲消除,需要在會議室內佈置多個麥克風,有時候是多個揚聲器。另一種可能的應用是在公共禮堂、集會,以及需要同步即時翻譯的場合。在大型會議室內,真正限制A2B 應用的因素是單根匯流排中的電纜總長,一般限制為40米。

Figure 2. Traditional audio installation in a conference room.
圖2. 會議室內的傳統音訊裝置。

在這些應用中,A2B收發器可用於簡化遠端音訊節點的佈線,同時提供一種具有可選電源分配的傑出數位傳輸方法。如圖2所示,之前連接這些遠端音訊節點的方法是使用遮罩電纜,由每個線對單向傳輸一個類比訊號,並透過直流適配器單獨提供電源。同時,使用A2B的單根雙絞線可以傳輸最多32個上游和/或最多32個下游高保真數位音訊通道和匯流排電源,如圖3所示;使用16位元數據時,匯流排中的通道不得超過50個。與傳統的類比方法相比,如果在會議系統中部署所需的A2B功能,確實能帶來很多優勢,包括簡化佈線、增加雙向高保真數位音訊功能等。

Figure 3. Using A2B for audio installation in a conference room.
圖3. 將A2B用在會議室內的音訊裝置中。

A2B收發器同步連接多通道晶片間音訊(I2S),可在節點之間15米的距離,以及在所有節點總長40米的電纜內傳輸脈衝碼調變(PCM)數據。它還將 I2S的同步、分時多工(TDM)特性擴展到連接多個節點的系統,其中每個節點都會獲取數據或提供數據,或者兩者兼備。除音訊內容外,該數據還包括控制功能;例如,A2B 收發器晶片上的GPIO(一個典型的A2B收發器上最多支援7條GPIO線路)可以連接到麥克風節點的LED上,並且可由主機遠端切換,以指示有活動的(即時)或無活動的(靜音)麥克風。

A2B匯流排是一種單主機、多從機系統,主控制器中的收發器用於主機。主機節點為所有從機節點產生時脈、同步和幀啟用訊號。主機A2B 晶片可透過控制匯流排(I2C)編碼,實現配置與回讀。A2B數據流程中內建該控制匯流排的擴展版本,可以直接讀取從機收發器的暫存器和狀態資訊,並實現跨距離I2C-到-I2C通訊。系統通電後採用搜尋發現機制,識別各個節點,並且構成TDM結構要求。所有從機節點按照從機0一直到系統中最後一個可用從機的順序依次發現。發現了所有的從機節點之後,對每個節點進行初始化,以便進行同步數據交換。圖4所示為具有四個節點的簡單A2B系統示例。主機程式在每個節點中註冊,以控制A2B匯流排上的數據流程量。在本例中,將從機節點0和N上來自數位麥克風和ADC的數據傳輸到主機節點,同時將來自主機節點的揚聲器數據傳輸到從機節點1上的DAC。如本例所示,A2B收發器也包含一個多通道PDM介面,用於直接連接脈衝密度調變的麥克風陣列。

Figure 4. Simplified A2B system with four nodes (master + 3 slaves).
圖4. 包含4個節點(一個主機節點,三個從機節點)的簡化型A2B系統。

每個從機節點的音訊通道數量可以單獨配置,最多32個上游通道和最多32個下游通道。可以使用8、12、16、20、24、28或32位元的數據插槽來匹配I2S/TDM數據字的長度,但是所有節點必須使用相同大小的slot。上游和下游可以選擇不同的slot大小。此外,12位元、16位元或20位元槽大小可以選擇性地透過A2B匯流排傳輸16位元、20位元 或24位元I2S/TDM字長的壓縮數據。音訊採樣頻率(fSYNCM)可以設定為44.1 kHz至48 kHz,所有節點同步採樣數據。從機節點支持1× (48 kHz)、2× (96 kHz)或4× (192 kHz)採樣速率(fS),每個從機節點可單獨配置。為了在從機節點上支持2倍和4倍採樣速率,主機節點必須在連接至主機的1× fSYNCM介面使用I2S/TDM 數據通道2倍和4倍的通道。A2B收發器還包括可靠的誤差檢測功能,透過16位元CRC來檢查控制數據和狀態數據。A2B收發器的另一個重要功能是故障診斷,收發器 可以檢測A2B電纜何時高壓短路、接地短路、電纜短路、電纜反向或存在開路連接。

在匯流排供電系統中,周邊電源電流消耗會直接影響到系統中的其他節點。重要的是,始終保持在熱封裝限值內,且不超過任何A2B匯流排節點的IVSSN和VIN的規格限值(內部切換在1.2 Ω IVSSN限值時為300 mA/100 mA,由收發器型號決定;最高提供9 V輸入電壓VIN)。A2B收發器晶片的數據手冊提供豐富的功率預算計算示例,圖5所示為一個由匯流排供電的系統的模型。

Figure 5. A dc power model for a system with local and bus-powered slaves.
圖5.包含本地供電和由匯流排供電的從機的系統的直流電源模式。

雖然一根基本的雙線電纜足以支援A2B操作,但正確選擇電纜和連接器則有助於其滿足業界常見的更嚴格的EMC測試要求。需要選擇合適的電纜,以便除了典型的光譜輻射範圍之外,還能提供傑出的電氣性能,以免在通訊頻率諧波下發生差分-共模轉換。

多種評估板可選擇,使得工程師在設計之前進行,全面測試和評估A2B元件的性能。以下是ADI提供的一些評估板的示例。

Figure 6. EVAL-AD2428WD1BZ, A2B master- or local-power slave node (I2S/TDM, 3 PDM mics).
圖6. EVAL-AD2428WD1BZ, A2B 主機或本地電源從機模式(I2S/TDM 、3個PDM麥克風)。
Figure 7. EVAL-AD2428WB1BZ, bus-powered A2B slave node (I2S/TDM, 2 PDM mics).
圖7. EVAL-AD2428WB1BZ,由匯流排供電的A2B從機節點(I2S/TDM、2個PDM麥克風)。
Figure 8. EVAL-AD2428WC1BZ, bus-powered A2B slave node (no I2S/TDM, 4 PDM mics).
圖8. EVAL-AD2428WC1BZ,由匯流排供電的A2B從機節點(無I2S/TDM、4個PDM麥克風)。
Figure 9. EVAL-AD2428WG1BZ, local-power A2B slave node (I2S/TDM, no PDM mics).
圖9. EVAL-AD2428WG1BZ,本地電源供電的 A2B從機節點(I2S/TDM、無PDM麥克風)。
Figure 10. ADZS-AUDIOA2BAMP, A2B class D amplifier module.
圖10. ADZS-AUDIOA2BAMP, A2B D類放大器模組。
Figure 11. SHARC® audio module: an expandable hardware/software platform for audio applications.
圖11. SHARC® 音訊模組:適合音訊應用的擴展硬體/軟體平台。

有關ADI提供的A2B技術的更多設計資源,請點擊 此處 參考。