ADALM2000:齊納二極體穩壓器

作者:ADI 顧問研究員Doug Mercer 及系統應用工程師Antoniu Miclaus

目的

穩壓器是一種讓負載上的輸出電壓可以保持恆定,而不會隨負載電流變化的電路。例如,負載可以是微控制器系統,而這就要求電源電壓保持恆定,即使其電流會隨著系統活動的變化而變化亦是如此。圖1所顯示的齊納二極體穩壓器提供了一種非常簡單的方法,來將負載電壓VL保持與齊納二極體的反向擊穿電壓至相同的值,其只要負載電阻RL保持在高於某一下限。電壓源VIN和電阻RS透過戴維寧(Thévenin)等效電路模擬了輸入電路特性,例如,將一個高電壓(如120 V交流電源)轉換為未經調節和濾波的較低直流電壓源。

材料準備

  • ADALM2000 主動學習模組
  • 無焊麵包板
  • 1個1 kΩ電阻(RS)
  • 1個5 kΩ可變電阻、電位計(RL)
  • 1個齊納二極體(1N4735或類似產品)

指導:

使用1N4735 6.2 V齊納二極體在無焊麵包板上構建圖1所示電路。使用AWG1(5 V恆定)和–5 V Vn用戶電源作為直流電源VIN。RL使用各種固定和可變電阻。

圖 1. 齊納二極體穩壓器
圖2.齊納二極體穩壓器麵包板電路

程序

步驟1

對於下列值的RL,使用Scopy電壓表(Scopy Voltmeter )測量VL以監視並報告負載電壓VL

  • 開路(請參見圖3)
  • 10 kΩ(請參見圖4)
  • 1 kΩ(請參見圖5)
  • 100 Ω(請參見圖6)
圖3.RL = 開路齊納二極體穩壓器波形
圖4.RL = 10 kΩ齊納二極體穩壓器波形
图5. RL = 1 kΩ 齊納二極體穩壓器波形
F图6. RL = 100 Ω 齊納二極體穩壓器波形

步驟2

透過以5 kΩ電位計來替換負載RL,並調節電位計,以確定VL保持在齊納電壓VZ的10%以內的RL的最小值。測量並報告設置的電位計電阻。該阻值與RS的值有何關係?

進一步探索

透過步驟2所述的操作,利用示波器通道2測量RS中的電流,並在示波器XY模式下繪製齊納二極體兩端電壓與電流的關係圖,研究齊納二極體的電流/電壓特性曲線。務必調整水平電壓範圍和偏移,以將6.2 V擊穿電壓包括在內。討論您的結果,尤其要討論齊納二極體與常規二極體的相似和不同之處。

驅動更大負載電流

正如我們在圖1的簡單齊納二極體穩壓器中看到的,最大負載電流是由電阻RS決定。另外,相對於最大電流,該電路在較小負載電流下的效率非常低,因為當負載中的電流較小時,額外電流會流入齊納二極體。相對於如圖2所示的穩壓電路,增加一個射極跟隨器或達林頓( Darlington)射極跟隨電流放大器可以大大提高穩壓電路的效率。

附加材料

  • 兩個NPN電晶體(2N3904和TIP31)
  • 兩個小訊號二極體(1N914或類似元件)
圖7.加入一個電流放大器級

指導:

D1使用1N4735 6.2 V齊納二極體,Q1使用2N3904或TIP31功率電晶體,在無焊麵包板上構建圖7所示的任一電路。Q2可以是2N3904,D2、D3可以是1N914。

增加二極體D2與齊納二極體串聯,用以部分抵消射極跟隨器Q1引起的額外VBE壓降。類似地,在達林頓配置中添加兩個二極體(D2、D3),同樣用來部分抵消達林頓跟隨器的兩個VBE壓降。

問題

使用圖1所示電路,計算VL值等於齊納電壓VZ 20%時的電阻RL

您可以在StudentZone blog學子專區部落格找到相關的問題答案。

Authors

Doug Mercer

Doug Mercer

Doug Mercer received his B.S.E.E. degree from Rensselaer Polytechnic Institute (RPI) in 1977. Since joining Analog Devices in 1977, he has contributed directly or indirectly to more than 30 data converter products and he holds 13 patents. He was appointed to the position of ADI Fellow in 1995. In 2009, he transitioned from full-time work and has continued consulting at ADI as a Fellow Emeritus contributing to the Active Learning Program. In 2016 he was named Engineer in Residence within the ECSE department at RPI.

Antoniu Miclaus

Antoniu Miclaus

Antoniu Miclaus is a system applications engineer at Analog Devices, where he works on ADI academic programs, as well as embedded software for Circuits from the Lab®, QA automation, and process management. He started working at Analog Devices in February 2017 in Cluj-Napoca, Romania. He is currently an M.Sc. student in the software engineering master's program at Babes-Bolyai University and he has a B.Eng. in electronics and telecommunications from Technical University of Cluj-Napoca.