Abstract
MAX16800测试板是一个简单的高亮度LED驱动电路板,专为驱动Osram、Lumileds、Nichia、Cree或其它LED驱动设计。测试表明,MAX16800适合用于汽车的内部和外部LED照明,以及商业和工业LED照明。
概述
40V、350mA,可调节的线性高亮度LED驱动器
MAX16800测试板是经过完全安装和测试的电路板,用于评估MAX16800高亮度LED驱动器。MAX16800的输出电流通过与LED串联的外部检流电阻设置。使能(EN)引脚允许连接一个宽范围的PWM亮度调节信号。MAX16800非常适合要求高压输入的汽车应用,能够承受高达40V的甩负载。
特性
- ±3.5%输出电流精度
- 内置调整管,低压差(<1.2V)
- +5V稳压输出,可以源出4mA电流
- 差分LED电流检测
- 关断时,具有极低的电源电流(12mA,典型)
- 低至204mV的电流检测基准有助于降低功耗
- 工作电压可低至+5V,满足汽车冷启动的要求
- 整形电路用于平滑波形边沿,降低PWM亮度调节的EMI辐射
电路板布局和连接
规格
Input Voltage | 6.5V to 40V |
LED Current (load Current) | 0.35mA to 350mA, set at 350mA |
Maximum Output Voltage | Input Voltage—0.6V (typ.) |
Short-Circuit Protection | Continuous |
Thermal Shutdown | 155°C (typ) |
PWM/ENable Pin Voltage | Up to 40V |
PWM Dimming Range | 100Hz to 1KHz (typ.) |

实际尺寸:2" x 1.25"
PCB顶层丝印层
PCB顶层
PCB底层
电路框图
元件列表
Reference | Part | Value | Manufacturer |
C1 | - | 0.1µ, 50V, 10%, Ceramic X7R, (0603) | - |
C2 | - | 0.1µ, 10V, 10%, Ceramic X7R, (0402) | - |
R1 | - | 0.56Ω, 1%, (1206) | - |
U1 | MAX16800ATE | Linear Adjustable, High-Brightness LED Driver | Maxim |
LED | Q65110A2922 | Golden DRAGON White LED (LW W5SG) | OSRAM Opto |
LED* | LXHL-MW1B | Luxeon Star/C White LED | Lumileds |
说明
VIN+: 将直流输入电源的正端连接到J1-1。
GND: 将直流输入电源的负端连接到J1-2。
LED+: 将串联LED的阳极连接到这个焊盘。使用外接LED时,断开板上的LED。
LED-: 将串联LED的阴极连接到这个焊盘。当使用外接LED时,断开板上的LED。
PWM/EN: 此引脚可以用于使能/禁用LED驱动器或用于连接PWM亮度调节信号。用跳线连接VIN+和PWM/EN引脚,将打开LED驱动器。关断LED驱动器时,则使用跳线连接PWM/EN引脚至GND。
在PWM/EN引脚和GND引脚之间作用一个PWM信号,可以在0至100%最大设置电流之间调节LED电流,改变PWM信号的占空比则会改变LED的亮度。将EN引脚连接到VIN时,也可以利用PWM信号对VIN+ (输入电源)进行斩波达到调节LED亮度的目的。
LED电流设置: 设置LED电流为350mA。LED电流可以通过改变R1的阻值,按照下式调整:ILED = VSENSE / R1。
电流可以通过在J2的LED和GND引脚之间添加外接电阻进行调整。当使用外部电阻时,必须确保R1断开。
可以在J2引脚之间接入示波器探头,以监控通过LED的电流。测得的电压除以R1,既为通过LED的电流。
线性亮度调节: LED的电流可以通过改变R1的阻值或在LED引脚增加一个偏移电压实现线性调节。可以在V5 REG与LED-和GND引脚之间接入电阻分压器产生偏移电压。
断开LED: 当驱动器运行时,断开LED连接,将不会损坏LED或驱动器。
功耗: 当IC功耗使结温达到155°C,热关断功能将会关断器件。可以在器件输入端添加一个电阻,或将一个电阻与LED串联,减小IC的功耗。电阻的额定功率必须高于I²R (I为输入电流或LED电流,R为所添加的电阻)。
V5: +5V稳压器可以为J4的其它元件供电。当EN引脚接GND时,V5输出关断,以减小静态电流。
接头位置功能说明
Jumper | Setting | Effect |
J2 | Open | R1 senses LED current |
J2 | Short | Device will internally current-limit to the maximum current set by the short-circuit current limit (800mA, max). This may cause LED damage. |
J2 | R1-removed; external resistor added to these pins | Current through the LEDs will be determined by the value of resistor on J2. |
J3 | No jumper | Will cause an undetermined voltage on the EN pin, which can enable or disable operation. |
J3 | Pins 1 and 2 shorted | Device enabled; LED current regulated |
J3 | Pins 2 and 3 shorted | Device disabled; in low-current standby, V5 turns off. |