|
Online Training On-demand training on Embedded Processors and DSPs. |
| Webcast: Targeting Analog Devices Blackfin and SHARC processors from MATLAB |
|
In this webcast, MathWorks and Analog Devices' engineers will demonstrate how a signal processing design, using an audio parametric equalizer as an example, can be designed in MATLAB and Simulink, tested through simulation, implemented on a Blackfin processor, and interactively tuned in real-time from a MATLAB GUI using the processor's Background Telemetry Channel (BTC). Duration: 1 hourView webcast now |
| Webcast: Analog Devices' SHARC ADSP-2146x Processors |
|
Learn about the newest member of Analog Devices' SHARC family, the ADSP-2146X. The family offers improved computing performance\power metrics,
enhanced memory options and code flexibility and optimization. The ADSP-2146X doubles the MIPS performance of the ADSP-2136X family and comes
with a robust peripheral set designed to enable a wide range of industrial applications.
Join Satya Simha, Senior Product Marketing Manager for SHARC DSP Products at Analog Devices Inc., for a detailed overview of the new ADSP-2146X family of SHARC DSPs including:
|
| Webcast: Advantages of SHARC Processors in Test/Measurement Applications |
|
Analog Devices SHARC® processors offer best-in-class performance for the given power and cost, creating a vast range of advantages in different
industrial environments where performance is critical. With a powerful engine for FFT and signal analysis and wide dynamic range processing for complex
computation, SHARC processors are ideal for optimizing test and measurement applications such as lab test equipment and power and process control systems.
Join David Miller, Applications Engineering Manager at Analog Devices, for a webcast covering the following topics:
|
| Webcast: SHARC Processor Family: Highest Performance Floating Point Processor under $30 |
|
The SHARC® Processor family makes floating point processing economical in applications where dynamic range is a key consideration
such as home and car audio, medical, industrial and instrumentation.
Join David Miller, Applications Engineering Manager at Analog Devices, for a webcast covering the following topics:
View On-Demand Webcast (17 minutes) |
|
1-Day Seminars and Workshops Workshops and seminars for those who want to evaluate the capabilities of ADI's high-performance embedded processors and development tools. |
| European ADI Embedded Processors Workshop by Silica |
Analog Devices' distributor Silica (an Avnet Company) offers a pan European ADI Embedded Processors Workshop series.
With dates in Germany, Spain, Italy, Netherlands and Belgium, engineers are invited to attend these workshops to
get the latest information on ADI Embedded Processor offerings, including the Blackfin Processor-based Silica
FireCracker Reference Design.
Duration: 1 Day Cost: Free |
| Location | Date |
| Berlin, Germany | 9 Sept 2009 |
| Braunschweig, Germany | 10 Sept 2009 |
| Bilbao, Spain | 29 Sept 2009 |
| Barcelona, Spain | 30 Sept 2009 |
| Torino, Italy | 6 Oct 2009 |
| Padova, Italy | 17 Nov 2009 |
| Modena, Italy | 18 Nov 2009 |
| Breda, Netherlands | 9 Dec 2009 |
| Brussels, Belgium | 10 Dec 2009 |
|
多日短训班 深入的技术培训,旨在通过讲解和动手练习帮助学员掌握有关嵌入式处理器和开发工具的知识。 |
| SHARC系统开发与编程 (ADSP-21368/9和ADSP-21375) |
|
教您如何利用SHARC®处理器ADSP-21368/9和ADSP-21375高效完成设计。学员还将使用最新的VisualDSP++开发工具(含汇编和C语言)进行动手练习。由经过ADI公司培训的Kaztek Engineering专家讲授。课程详情。
时间: 3天半 语言: 英语 费用: 提前注册可优惠6%培训费: $1500 USD(北美)/ $1850 USD(欧洲)- 确认/取消决定日期之前缴费 $1595 USD(北美)/ $1975 USD(欧洲)- 确认/取消决定日期之后缴费 注意: 确认/取消决定日期为短训班开始日期前三周。 |
| 地点 | 日期 | 注册 | |
| Munich, Germany | 27-30 Oct 2009 | 立即注册 | |
| Munich, Germany | 1-4 Dec 2009 | 立即注册 |
可根据需求开办其它SHARC处理器多日短训班。若需要所有短训班的列表,请访问 Kaztek Engineering网站。
Today many signal processing and control algorithms developed in MATLAB and Simulink are implemented on Analog Devices
Blackfin® and SHARC® processors.
Analog Devices' distributor Silica (an Avnet Company) offers a pan European ADI Embedded Processors Workshop series.
With dates in Germany, Spain, Italy, Netherlands and Belgium, engineers are invited to attend these workshops to
get the latest information on ADI Embedded Processor offerings, including the Blackfin Processor-based Silica
FireCracker Reference Design.