POWER MANAGEMENT DOWNLOAD TOOLS Excel-based design tools and parametric selection for power

With the exception of the Supervisor Parametric Search, the following stand-alone tools generate a power supply design complete with a schematic, bill of materials, and performance specifications including efficiency based on the user's preference for size, efficiency, and cost.

IMPORTANT: You must enable macros when Microsoft Excel asks you as the file is being opened.

The same tools (ZIP files) are available from ADIsimPower or Supervisor Parametric Search.

Note: Microsoft Excel is dependent on the language setting Microsoft Windows for the indication of a decimal point. Issues may arise when some of these files are read/run in Excel of another language that does not use decimal point notation (such as "2.7") and uses instead decimal comma notation (such as "2,7"). The the temporary workaround is to change the language of Microsoft Windows to English. [Control Panel->Region and Language->Format]. The specific error comes from the Excel Rank command that is used by just a few tools and that does not gracefully handle decimal notation of the opposite sort suddenly in a "smart" Microsoft Excel format conversion to the regional language when opened.

提供意见反馈 X
content here.
content here.

提供意见反馈

关闭