新闻
- 2009年01月12日 FUJITSU TEN公司采用ADI公司SHARC DSP实现汽车音响系统的声学空间控制
- 2008年11月13日 新款SHARC®浮点DSP处理器提供业界最高性能
- 2008年10月14日 ADI公司的新一代SHARC®处理器满足专业音频的所有需求
新产品
-
ASYNCHRONOUS SAMPLE RATE CONVERTER (ASRC)
Asynchronous Sample Rate Converter (ASRC) is used for audio sampling rate conversion in both consumer and professional applications. The ASRC software module supports a variety of sample rate configurations. The ASRC software module can be used to change the sampling frequency in small steps which vary with time without producing any audible artifacts in the output, during the change. Such a time More
-
USB EZ-EXTENDER FOR BLACKFIN AND SHARC EZ-BOARDS/EZ-KIT LITES
The Blackfin SHARC USB EZ-Extender plugs onto the expansion interface of the ADSP-BF518F, ADSP-BF526, and ADSP-21469 EZ-Board and EZ-KIT Lite’s. The EZ-Extender aids the design and prototyping phases of the processor targeted applications and extends the capabilities of the evaluation system by providing a connection between the asynchronous memory bus of the Blackfin/SHARC processor and a USB More
-
SHARC AUDIO EZ-EXTENDER FOR 214XX EZ-BOARD/EZ-KIT LITES
The SHARC Audio EZ-Extender provides users the ability to evaluate audio application on the ADSP-214xx EZ-Board/ EZ-KIT Lite. Software examples are provided in the latest update of VisualDSP++.
The EZ-Extender consists of three Analog Devices AD1939 audio codecs and provides 24 channels of analog audio out, 12 channels of analog audio in. The primary codec operates in both in I2S and TDM More
- 订阅新产品资料