COMPILATION OF ADI SOLUTIONS

Highlight ---A System Solution for IEDs Based on IEC61850
A smart grid is an electrical grid that uses information and communications technology to gather and act on information, such as information about the behaviors of suppliers and consumers, in an automated fashion to improve the efficiency, reliability, economics, and sustainability of the production and distribution of electricity.…
More…
   INDUSTRIAL & INSTRUMENTATION
A System Solution for IEDs Based on IEC61850
Download
A smart grid is an electrical grid that uses information and communications technology to gather and act on information, such as information about the behaviors of suppliers and consumers, in an automated fashion to improve the efficiency, reliability, economics, and sustainability of the production and distribution of electricity. The intelligent…
More…

2-Wire Loop-Powered Transmitter Solution
Download
Modern field instruments, otherwise known as smart transmitters, are intelligent microprocessor-based field instruments that monitor process control variables (e.g., temperature, mass flow rate, and pressure). The incorporation of extra intelligence, functionality, and diagnostic capabilities, while developing a system which can operate effectively within…
More…
Ultrasonic Non-Destructive Testing
Download
Non-destructive testing (NDT) is a wide group of analysis techniques used in science and industry to evaluate the properties of a material, component, or system without causing damage or permanent alteration. Because it is a valuable technique that can save both money and time, it is widely used in product evaluation, troubleshooting, and research in many fields…
More…
Spectrum Analyzer Solutions
Download
Spectrum analyzers are used to measure the magnitude of the input signal versus frequency within the full frequency range of the instrument. Distortion, harmonics, bandwidth, and other spectral components of a signal can be observed by analyzing the spectrum of electrical signals that are not easily detectable in time domain waveforms.…
More…

ADI Gas Detector Solution Based on NDIR and PID
Download
This is the second article on gas detectors from ADI, which contains the NDIR (non-dispersive infrared) gas detector solution and the PID (photoionization) gas detector solution. The first article describes a micro-power toxic gas detector based on an electrochemical sensor (see Design Resources at end of this article for additional information)…
More…
ADI Micropower Toxic Gas Detector Solutions Based on Electrochemical Sensors
Download
Toxic gases exist in many industrial environments, like oil wells, mining, plastics manufacturing, paper making, and so on. With the increasing concerns of personal safety, the demand for low power portable toxic gas detectors is rapidly increasing so that workers can carry them in the field or they can be installed in the field. Most portable low power toxic gas detectors…
More…
Motor Control Solutions
—Servo Control
Download
For motor control solutions, Analog Devices offers a complete product portfolio including data converters, amplifiers, embedded processors, iCoupler® digital isolators, and power management devices. Enhanced performance and system integration enable innovative design topologies, which add value and help differentiate our customer’s systems…
More…
Li-Ion Battery Test Equipment Solutions
Download
Lithium-ion (Li-ion) batteries offer many benefits over other battery chemistries. For example, when compared with nickel-metal hydride batteries or nickelcadmium batteries, they are lighter, do not suffer from memory effect, and have a lower self-discharge rate. Li-ion batteries have been widely used as rechargeable batteries in modern electronic devices…
More…

Electromagnetic Flow Meter Solutions
Download
The operating principle of the electromagnetic flow meter is based on Faraday’s law of electromagnetic induction. When the magnetic field direction perpendicular to the conductor cutting magnetic line is speed V, both ends of the conductor will be induced by a certain force E, and the liquid flow rate change can be calculated by detecting the value of the force……
More…
RF Signal Source Solutions
Download
RF signal sources are used to create test waveforms at radio frequencies. Some of its common applications are to test if a new radio platform works or if the handsets coming off a production line are performing as they should. RF signal sources can be used to create simple waveforms such as sine waves or complex, modulated waveforms that look like the return…
More…
Energy - Protective Relay Platform for Power Distribution Systems
Download
In the modern automatic power distribution system, more and more intelligent electronic devices are used to monitor the power quality and quickly isolate any fault from affecting the overall grid operation. The architecture of such devices is mostly composed of processor, multichannel ADC, signal condition circuit, power supply…
More…
Renewable Energy
—Solar PV Solutions
Download
Analog Devices leads the industry in highly accurate and precise signal measurement and control by delivering cost competitive, high quality ICs for reliable metering, measurement, and control. These products are used in renewable energy, electrical power transmission, and distribution applications, as well as electric, gas, and water metering…
More…

PLC (Programmable Logic Controllers)
Download
Comprised of power supplies, CPUs, and multiple analog and digital I/O modules, a PLC system controls, actuates, and monitors complex machine variables; the PLC is designed for multiple input and output arrangements, extended temperature ranges, immunity to electrical noise, and resistance to vibration and impact.…
More…
     

   AUTOMOTIVE
HEV/EV Li-Ion Battery Management Solutions
Download
The automotive industry is transitioning from nickel-metal hydride battery solutions to lithium-ion (Li-ion) due to Li-ion’s superior energy and power capabilities in hybrid and pure electric vehicles. Typically micro/mild hybrid vehicles require batteries that can deliver between 60 V to 200 V. NiMH still has some advantages at these lower voltage and energy requirements…
More…

Infotainment Head Unit Solutions
Download
Infotainment head unit systems bring comfort and convenience to the driver through audio/video playback, navigation, and telematics. Typical functions included in the system are AM/FM/digital/satellite radio, CD/DVD playback, multimedia accessories, rear seat entertainment, navigation, camera integration, bluetooth connectivity, and telecom connectivity…
More…
ADAS Vision Solutions

Download
In many ways, vehicle safety can be greatly enhanced by vision-based ADAS systems (advanced driver assist systems). By installing rear/front/side cameras and vision processing ECU, multiple features can be implemented to assist the driver in advance. Popular applications include LDW (lane departure warning), HB/LB (high beam/low beam adjust)…
More…
 

   HEALTHCARE
Medical Ultrasound Solutions
Download
By transmitting acoustic energy into the body and receiving and processing the returning reflections, ultrasound systems can generate images of internal organs and structures, map blood flow and tissue motion, and provide highly accurate blood velocity information…


More…

Activity Monitoring Solution
Download
As global healthcare costs increase, more and more emphasis is being placed on personal health management as a means to proactively reduce the risk of health issues and, therefore, reduce the number of doctor and/or hospital visits. Tracking one’s daily activity is growing in popularity due largely to its simple yet effective…

More…
Typical Module in
Patient Monitor Pulse Oximeter
Download
The pulse oximeter noninvasively measures oxygen levels in the blood. It is measured as a percentage of full saturation level and is expressed as a single number known as the saturated percentage of oxygen, often referred to as SpO2. The measurement is based on the light absorption characteristics of hemoglobin in the blood. Oxygenated hemoglobin (HbO2)…
More…
Electrocardiogram (ECG) Solutions
Download
Electrocardiogram (ECG) systems record the electrical activity of the heart over time by measuring electric potentials on the surface of living tissue. A biopotential electrode is used to pick up heart signals from specific locations on the body. The differential voltage between two electrodes, or the differential voltage between one electrode…
More…
提供意见反馈 X
content here.
content here.

提供意见反馈

关闭